NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello,I'm looking for some example code on using the built in RTC for the STM32WB55 to get a timestamp in UNIX UTC Time in milliseconds. Or the number of milliseconds since January 1st 1970.If anyone has a simple example on how to accomplish this I w...
Good morning......I am using the ADC with 2 channels (Ch 9 and Ch 10). I am using an LPTIM to take these samples every 15ms. I have the ADC callback (HAL_ADC_ConvCpltCallback) to interrupt on 'End of sequence of conversion' (per .ioc --- or so I thin...
We have encountered issue with WB55 BLE firmware where it doesn't accept AD_TYPE_COMPLETE_LOCAL_NAME longer than 9 characters We have reproduced that issue on p2pServer example where we've modified local_name to be "123456789" all is OK.static const ...
Hi everyone.I need to activate a different USB device (one only, no multi role) at startup, depending for example on a GPIO status. I have two versions of an application on a STM32WB55 Nucleo board working as MSC in a version and CDC in the other. I ...
Hi,I'm creating a custom PCB for the STM32WB55 with BLE functionality and was wondering if in order to use BLE, do I need to include a 32Khz Oscillator on pins PC14 and PC15? I am assuming I do, but did not see anything definitive in the datasheet.T...
We are trying to bring up LoRaWAN Class B on NUCLEO-WL55JC1 platform. We enabled LoRaWAN End Node with the following,#define LORAWAN_DEFAULT_CLASS CLASS_B => in lora_app.h#define LORAMAC_CLASSB_ENABLED 1 => in lorawan_conf.hWe have LoRa Se...
Thanks for your participation to the STM32WB Bluetooth and ZigBee Mesh Webinar .Recording of the session is here.Following is a collection of questions received during the Q&A session we were unable to answer in real time due to time constrains.For d...
Thanks for your participation to the STM32WB Bluetooth and ZigBee Mesh Webinar .Recording of the session is here.Following is a collection of questions received during the Q&A session we were unable to answer in real time due to time constrains.For d...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.