2022-01-03 8:52 AM
I think this is more of a c programming question rather than a MCU question, but I figured I would ask anyway. I am trying to append the chip ID from an STM32WB onto the BLE local name for my application and am having trouble figuring out how to do this.
my local name is a const char *name = TEST
My chip id is a uint32_t Device_ID which was read from the device register (0x1FFF7580).
lets say the Device_ID = 0x8BE4...
How can I combine these two such that my local name ends up being "TEST 8BE4"
Solved! Go to Solution.
2022-01-03 11:22 AM
This should do it:
sprintf(name, "TEST %04X", id);The length of the resulting string can be calculated with strlen(name).
2022-01-03 11:11 AM
char name[32]; //or how is max name len
sprintf(name, "TEST %x", id);
or
sprintf(name, "TEST %08x", id);
2022-01-03 11:22 AM
This should do it:
sprintf(name, "TEST %04X", id);The length of the resulting string can be calculated with strlen(name).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.