STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Has anyone tried to update firmware over the air (FOTA) using the example code provided by STM (LoRaWAN_FUOTA) in STM32WL software package?

For this , I am using STM32WLJC1 Nucleo as my end node device.I was able to generate the binaries as suggested in AN5554. I want to know how I can fragment this binary as required by LoRaWAN® Fragmented Data Block Transport Specification v1.0.0 and u...

VA by Associate II
  • 1945 Views
  • 2 replies
  • 1 kudos

Zigbee Security Key Error

Hi,I'm trying to form a user defined network, but i always get the next error when I receive a response: [M0] [00000017.002][PLATFORM]                  aps_sec_build : Unable to encrypt (no security material for 0x0080e125001b6836 with key type = 0x0...

Pablo1610 by Associate II
  • 1241 Views
  • 0 replies
  • 0 kudos

I got some issues on the P-NUCLEO-STM32WB to upgrade the FUS

Good afternoon,Test1: I want to upgrade the FUS (at the moment it is FUS version 0.5.3.0) to upload next, the FTD thread stack. But when I upload the stm32wb5x_FUS_fw_for_fus_0_5_3.bin (from the last version of Patch-CubeWB: FUS version 1.2.0) with S...

TTAIL.1 by Associate II
  • 2990 Views
  • 6 replies
  • 0 kudos

How to add I2C to I-CUBE-LRWAN SDK SubGHz_Phy example? The reason I'm looking for it is that I was able to run SubGHz_Phy successfully but I'm unable to add the I2C to run successfully.

It's very hard to add it without instructions to not break existing infrastructure with LoRa.When I run simple example generated from classic .IOC file I got the I2C running without a problem.The board I'm using: Murata Type 1SJ

STM32WB5MMG connection couldn't finish

I was testing the STM32WB5MMG on the new U585 IOTA discovery kit and I'm facing some issues.I generated a project using STM32CubeIde with the MXEditor. After enabling all the default peripherals and changing the example config of BLE, some points are...

XPera.2 by Associate
  • 1155 Views
  • 1 replies
  • 0 kudos

"Debugging" crashes program

Running a program on the stm32wl nucleo board works fine, but if I enable debugging it alwaus crashes. This does the same thing on my custom board. It's always the same signal handler

0693W00000KbVNZQA3.png
Bstan.1 by Associate
  • 888 Views
  • 1 replies
  • 0 kudos

Wakeup procedure via BLE for system in low power mode

Hi,I am currently working on a bluetooth application developing it on Nucleo STM32WB55 (FW version V1.13.1, BLE Stack Full).If the system is in a low power state, STOP2, can it be woken up via bluetooth?If so, is this awakening established by any kin...

SDi B.2 by Associate II
  • 1849 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.