2022-03-08 1:21 AM
Hi,
I'm trying to form a user defined network, but i always get the next error when I receive a response:
[M0] [00000017.002][PLATFORM] aps_sec_build : Unable to encrypt (no security material for 0x0080e125001b6836 with key type = 0x00).
The configuration parameters for the coordinator are the next ones:
config.extendedPanId = 0x400;
config.panId = 0x7171;
config.shortAddress = 0x7171;
config.networkManagerAddress = 0x7171;
config.startupControl = ZbStartTypeForm;
and the ones for the End devices:
config.startupControl = ZbStartTypeRejoin;
config.networkManagerAddress = 0x0001;
config.panId = 0x0001;
config.shortAddress = 0x0001;
config.extendedPanId = 0x400;
Do I have to configure more parameters to form a user defined network?
Thanks,
Pablo
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.