STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 302 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4120 Views
  • 0 replies
  • 3 kudos

COMP1 HW or SW problem recovering from STOP2 mode

Hello everyone,​I discovered a problem with the STM32WLE5CCU6 using the comp1 on stop2 mode.​More specifically, when the debug is enabled on stop2 mode using the command HAL_DBGMCU_EnableDBGStopMode() the comp1 is working and I get all the peaks of t...

0693W00000Nr9LfQAJ.png 0693W00000Nr9LpQAJ.png 0693W00000Nr9NlQAJ.png

STM32 BLE

Hello everyone,We are planning to use ST products in our new BLE-supported projects. But I am not sure which product is suitable for this.As I see, there are some BLE chips connectable with SPI and there are SoC ICs like STM32W.I am not sure which is...

Reading 1 byte only in SPI half duplex

Hi everyone,I'm using a P-NUCLEO-WB55 for an SPI application with a CMT2219A (HF receiver) which works in Half duplex.I try to read its configuration registers by sending the address with the R/W bit set, then reading the bus by clocking during a byt...

0693W00000NqsGdQAJ.png 0693W00000NqsFuQAJ.png
Tøm by Associate II
  • 2265 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.