NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I want to have 4 diveces as peripherals, each of one with a button, that they comunicate the button state to a 5th device (a Central) in a determinated period of time. The peripfherals should turn off the anttena (or save battery us much as they can)...
Hello,The MCU used in our project is STM32WBCEU (LQFP48).I am going to download the BL stack binary in the form of Firmware Upgrade through STMProgrammer >> FUS page.The problem is that I face a "Wrong address" error.Where can I find the Start addres...
Very new but excited to start an IoT project here. I have a WL55JC1 and IKS01A3. I followed https://www.youtube.com/watch?v=9s8XiABakuQa and managed to get some widgets connected to Cayenne dashboard, but I can't add anymore widget as devices are gre...
Hello!I have a question - I'm working on interfacing with the STM32WB5M module on the B-U585I-IOT02A. From what I understand, the STM32WB5M module is already flashed with an example for AT commands (in the STM32Cube_FW_WB_V1.13.3/Projects/P-NUCLEO-WB...
See attached clocking setup. When I run this, BLE is unreliable. I am running STM32WB55CGU6 in server/peripheral mode. For example, sometimes on power up advertising is occurring and sometimes it does not. And if advertising does work, connecting ...
I'm using STM32WB55 and communicating with a program using Windows BLE APIs. My system affords BLE 5.2 version and I know it affords 2 Mbps.However, I don't know how to change the BLE setup in the microcontroller and my program.Currently, my microcon...
I am trying to immigrate my project on STM32WB55RGV to STM32WB5MMGH. Now I am using last firmware package V1.13.3 instead of 1.10.0 that used for STM32WB55RGV.I updated FUS (FUS V1.2.0) and BLE_stack_full_fw. I am trying to connect STM32WB55RGV but i...
/*--------------------------------------------------------- * Shutdown *--------------------------------------------------------- *//* This API moves the stack to shutdown mode, used in case of a sleepy end device to conserve power. */void ZbShutdown...
I have to projects based on FreeRTOS. One is st example and one is generated by me from example .ioc file. All of the files in projects are the same (including FreeRTOS middleware directory). In the projects there is a task called periodically which ...
I'm using STM32WL V1.2.0 and trying to generate LoRaWAN End Node FreeRTOS application from .ioc file and make it work but I met some issues with sending data packets periodacally. After succescul join procedure device sends only one data packet. Afte...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.