NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello everyone,I hope are in the right forum ;)I want to migrate my existing TCP-WLAN based MCU application which acts as a data server with a proprietary protocol. The application comes very close to standard Posix TCP handling.Each connection is ha...
Hello everybody,I started to use ZigBee stack v1.14.0 and ran into an issue of adding temperature measurement server cluster (and also other clusters having reportable attributes).Our system has many running activities so for the first time I thought...
I would like to run the STM32WB55 BLE_TransparentMode on my custom application board, but first I need to re-assign the pins used for LPUART1. However, any code generation from CubeMX, even without making any modifications, causes hundreds of compile...
I'm trying to create a Makefile-based project for the STM32WL55CCUx microcontroller but it's not possible.Why is it disabled? Is there a workaround?Thanks in advance.
Hi, I have a small problem with the zigbee strack i hope someone could give me an direction for.When I boot up I get an error just after it initialized the CPU2(M0).static void APP_ZIGBEE_StackLayersInit(void){ APP_DBG("APP_ZIGBEE_StackLayersInit");...
Hello,While using the RTC_BKP registers with HAL_RTCEx_BKUPWrite seems all right, the definition of the registers in stm32wb55wxx.h are not. Maybe they should not be present, or they should be fixed, but having symbols defined that do not lead to wha...
We watch "HCI_DISCONNECTION_COMPLETE_EVT_CODE" event in "SVCCTL_App_Notification" function. When use DC power supply for STM32WB module, there is no problem. Our STM32WB application can receive "HCI_DISCONNECTION_COMPLETE_EVT_CODE" message from BLE s...
I downloaded the STM32WB MCU Fw pack through https://github.com/STMicroelectronics/STM32CubeWB.git. Then, I used STM32IDE v 1.10.1 to compile BLE_HeartRateFreeRTOS project. It is complied successfully. Then, I used Device Configuration Tool to updat...
Hi guys, I am using HSDatalog (v.1.4.0) with ST BLE Sensor App (4.16.1). I found one issue that the SensorTile.box FW got stuck if I click Start/Top too fast in ST BLE Sensor App. I did some debug and found it got stuck in the following code in hci_t...
Hi,Once I flash the base firmware(STM32cube_FW_WL_V1.0.0) in the RAK3172 module, I view the serial print. It displays Europe frequency… then I open the firmware(STM32cube_FW_WL_V1.0.0) and check the file named lora_info.c… in the file Europe and US r...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.