NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
We are starting a project using STM32WB MCU. We would like to minimize the power consumption while in sleep, but able to wake it up via BLE command. From the document AN5071(STM32WB ultra-low-power features overview) it says "Wakeup from this mode ca...
Hello, I need to broadcast data between multiple STM32WB55 boards in a mesh using Zigbee. So I figured trying to make the APS Message example bi-directional (so both sides can send a request) would be a good starting point. So basicly I copied every...
Hi Sir:I try to builld a project with unicast/broadcast function with custom message payload on NVM example. But, I found that ZbZclMsgClient/ZbZclMsgSever can't use the following code to broadcast message.Is there any issue to broadcast by ZbZcl...
Hi I'm right now using the Nucleo-WB55RG as a Peripheral device to which the central (tablet) connects. I built most of my codebase with the CubeMX Code Generator – that means I defined all of my services and characteristics in the GUI choosing the B...
Currently, I am working with an IoT application on the board Nucleo-WL55JC1 with the sensor BME688. The example I am using is LoRaWAN_End_Node downloaded from STM32Cube MX. What I did: I initialized the the BME688 and set up some configuration after ...
Hi, I'm new to stm32 dev, and the stm32cubeide.We want to use the NUCLEO-WL55JC2 to try out the lorawan capabilities. No problem there, the example works just fine. ( would be interested in the LoRaWAN_End_Node_DualCoreFreeRTOS example)butThe project...
Hi all,I try to implement a ZigBee device that acts as a Touchlink Target.My hardware is a STM32WB5MMG module. My debug UART is the LPUART1, no other UART configured.I use the STM32CubeMX 6.6.1 to generate the project and STM32CubeIDE 1.10.1 to compi...
Hi there,I am using an STM32WLE4C8 with FSK and I am trying to determine the offset between the internal carrier frequency and an incoming carrier frequency. This offset will be used to calibrate my device using a high accuracy incoming preamble and ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.