2022-08-18 5:35 PM
I downloaded the STM32WB MCU Fw pack through https://github.com/STMicroelectronics/STM32CubeWB.git.
Then, I used STM32IDE v 1.10.1 to compile BLE_HeartRateFreeRTOS project. It is complied successfully.
Then, I used Device Configuration Tool to update the Pins for USART1 to PA9 and PA10 by accessing BLE_HeartRateFreeRTOS.ioc in the IDE. Besides this change, I had no other changes in Device Configuration Tool.
After I saved the change, the code was automatically updated. However, when I complied it again, it shows a lot of errors as the attachment.
I do not expect the change of Pins configuration will cause the whole project fail to compile. I also attached the git diff after the Device Configuration Tool change the code for the analysis.
Any comments are welcome!
Thanks!
Solved! Go to Solution.
2022-08-22 7:55 AM
Hello,
Indeed, when you regenerate the BLE_HeartRateFreeRTOS project for CubeIDE using CubeMX tool, there is build errors due to duplicate files inside CubeIDE project structure. To solve the issue, I recommend you to delete all files in BLE_HeartRateFreeRTOS\STM32CubeIDE folder and then regenerate the project using CubeMX.
Best Regards
2022-08-22 7:55 AM
Hello,
Indeed, when you regenerate the BLE_HeartRateFreeRTOS project for CubeIDE using CubeMX tool, there is build errors due to duplicate files inside CubeIDE project structure. To solve the issue, I recommend you to delete all files in BLE_HeartRateFreeRTOS\STM32CubeIDE folder and then regenerate the project using CubeMX.
Best Regards
2022-09-05 5:50 PM
Thanks. It is working now.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.