NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Details:TX Power on Board: 14dBm (LP)Omnidirectional TX antenna (on board): 2dBiDirectional RX antenna (LPDA): 4dBiDistance: 0.5m free space with minimal interference in labFrequency: 868MHzFSPL (868MHz @ 0.5m) = -25dBExpected P_ in RX: -5dBmMeasure...
Hello ST team,We're having an odd SPI bug with our custom board.We made a board based on the STM32WB55, everything seems to work fine except for this issue.We're trying to use the spi in mode 0 (CPOL=0 CPHA=0) , but we can't make it work.We have thes...
Hello community,I am designing the STM32WL module for the EU868 (south Africa) region based on the LoRAWAN application. As per the datasheet of stm32WL, the max power used in transmitting is 14 dBm @ 868MHz, so with the reference from the Lora-allian...
Hi,I am using LoRa-E5 mini board from seeed studio (https://www.seeedstudio.com/LoRa-E5-mini-STM32WLE5JC-p-4869.html)To program it using STM32CubeIDE, do we need to connect it to pc using ST-Link or we can simply program it via Type C cable?
I am trying to get the simple ranging example code for the 53L5A1 to work on the WB55RG board but I keep getting a timeout error.The text output the example code outputs is "L53L5A1_RANGING_SENSOR_Init failed. Check you're using ONLY the center devic...
Need the I2C Detailed driver code which contains I2C Read/Write functionalities with DMA.Could anyone provide the code base it useful to us.Regards,Srinivas.V
Hi allSTM32WB55RG nucleo board zephyr (3.0)When BLE stack is enabled, it becomes halt.Can't I use LSI clock to make the BLE stack run ?We made a sample board, but We didn't attach an LSE.So. use LSI clock. If We use LSE in nucleo , it will behave...
HIMy STM32WB55 is configured as central and peripheral role.For debugging, Is it possible to establish an internal connection between them?Running two tasks to handle each app.Cheers!
HiI`m using PNUCLEOWB55 Board for testing USART1 interrupt communications.I have started a project from scratch using CubeID 1.10.1 and choosed PA9 and PA10 as TX/RX respectively with following configuration 115200Baud, WordLen 8bits(including parity...
Hi all,I would like to build a board with wireless module STM32WB5MMG.I'm using kicad and it is really difficult to insert a track for pin 84 (GND) in the central pads due to cad limitations with this BGA footprint. I would like to use only the exter...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.