2022-11-17 2:01 AM
Hello community,
I am designing the STM32WL module for the EU868 (south Africa) region based on the LoRAWAN application.
As per the datasheet of stm32WL, the max power used in transmitting is 14 dBm @ 868MHz, so with the reference from the Lora-alliance (PAGE 27) document given below, we are selecting Low power mode for RF.
Because for high power the maximum power for the transmitter is +22dBm and the minimum is +14dBm, which is not convenient as per the Lora alliance.
Please suggest a suggestion for this or correct me if I am wrong.
https://www.st.com/resource/en/datasheet/stm32wle5cc.pdf
https://resources.lora-alliance.org/technical-specifications/rp2-1-0-3-lorawan-regional-parameters
2022-11-23 6:21 AM
Hello @pragnesh ,
If you only select the region EU868, the max TX Power and the Max EIRP will be define. They are in line with the lora alliance specification for this region.
I suggest you to look for the file "RegionEU868.c" you will find here "Middlewares\Third_Party\LoRaWAN\Mac\Region" that describe the EU868_MAX_TX_POWER, EU868_DEFAULT_MAX_EIRP.
You can also refer to this post, and more specifically to my answer (the table 10 and the text below)
I hope this will help and answer your question.
Regards
Louis
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.