STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Invalid Teseo LIV3FL reading using STM32 Nucle-WL55JC1

I'm planning to make a GPS tracker using  Teseo LIV3FL as a slave device and STM32 Nucle-WL55JC1 MCU with I2C communication protocol. The I2C reading is working (I assumed it works since I'm receiveing some data), but the problem is when I take one o...

0693W00000WJxBiQAL.png 0693W00000WJxBnQAL.png
AFidi.1 by Associate II
  • 1222 Views
  • 2 replies
  • 0 kudos

Resolved! What does TSC_IOASCR do?

What does the TSC_IOASCR register do?Checked the reference manuals for STM32 WB35xx/WB55xx (RM0434) and F0xx (RM0091) and only get the following information: What's the behaviour of this setting for pins in the various modes (unused, sampling, channe...

0693W00000WJufQQAT.jpg
DK.6 by Associate II
  • 1722 Views
  • 1 replies
  • 0 kudos

FUS_STATE_ERROR_IMG_NOT_AUTHENTIC isuue

Hi, i'm trying to update stack via internal firmware. Our device based on STM32WB55: Device ID  : 0x495 Revision ID : Rev Y Device name : STM32WB5x Flash size : 1 MBytes Device type : MCU Device CPU : Cortex-M4 BL Version : 0xd5S...

0693W00000WIweSQAT.png
Yeti by Associate II
  • 2663 Views
  • 6 replies
  • 0 kudos

STM32WB55 boot mode issue

Hello!There is a board with 2 MCUs, one of them is STM32WB55, second is STM32L4Q5. I need to launch both in boot mode and load firmware over UART. When L4Q5 is in boot mode and UART1 is configured (as mentioned in AN2606) I upload firmware in this MC...

DHunt.2 by Associate II
  • 1369 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.