NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi,I'm Using stm32wb5mm-dk with I2S mic to capture audio and using TAS2563 I'm playing the captured audio. The data from the mic is transmitted and played using DMA. Now I want to transmit the I2S mic data using BLE. I used notification method using ...
Hi, I want to develop a basic Zigbee end device.After having successfully programmed a STM32WB55 Nucleo with the example Zigbee_OnOff_Server_Distrib, I tried to use CubeIDE to setup from scratch my own device. I am unable to set CFG_DEBUG_TRACE, as i...
Would like to update the ble stack of stm32wb55 to 1.15.Do old commands from stack 1.13 are supported?And which parameter describes the stack version:APP_DBG_MSG("Wireless Firmware version %d.%d.%d\n", WirelessInfo.VersionMajor, WirelessInfo.VersionM...
I connected my STM32WB5M DK with USB DFU mode according to manual and description.When i want to read or write the opt area over the cli and i got the error:Error: OTP programming is currently not supported on MCU devices What does it mean it is curr...
But I am not able to disconnect. Can someone please help me with how to disconnect from the server?
We made custome PCB board using STM32WB5MMG. We tried (489) BLE Security with STM32WB - 04 Simple BLE application generated from CubeMX - YouTube, and also we followed repository example too. We enabled the necessary settings which is mentioned above...
Using a sample example from your database code.Compatible with stack 1.15.0 (that is the stack I am running)STMicroelectronics ST-LINK GDB server. Version 7.1.0Copyright (c) 2022, STMicroelectronics. All rights reserved.Starting server with the follo...
I have a board P-NucleoWB55 and I'm trying to acquire a signal with external clock, very similar to uart, I tried with usart in slave mode without succcess, I tried with spi slave without success.Now I'm trying to trigger a DMA transfer with a timer ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.