2022-11-17 10:39 AM
Hello.
I'm trying to run this LoRaWAN FUOTA code: github.com/ SylvainMontagny/STM32WL/tree/main/STM32WL_FUOTA (that's the Single-core project on the Application Note AN5554), but i get the following error:
c:\st\stm32cubeide_1.9.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.0.202111181127\tools\arm-none-eabi\bin\ld.exe: cannot use executable file as input to a link 'C:/Users/USER/Downloads/STM32WL-main/STM32WL_FUOTA/Projects/NUCLEO-WL55JC/Applications/LoRaWAN_FUOTA/1_Image_BFU/STM32CubeIDE/Debug/se_interface_app.o' as input to a link
I've linked the "se_interface_app.o" file in Properties > C/C++ build > Tool Settings > MCU GCC Linker > Miscellaneous > Additional Object Files, but it didn't help.
How can i solve it? Any suggestions?
Thanks in advance :grinning_face:
2022-11-23 1:52 AM
Hello @PGior.2
Could you try with the example of the official STM32Cube_FW_WL_V1.2.0 under "Projects\NUCLEO-WL55JC\Applications\LoRaWAN_FUOTA" please and check if you have the same error.
Let me know if this help you.
Regards
Louis
2023-02-06 6:22 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.