STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Why STM32WB5MM-DK OLED Display stops P2pClient code working

Hi,I have a project where im using the STM32WB5MM-DK to develop code to act as a ble P2P client. I have the development board setup as a P2P client and the code is working fine. but when introducing the code to initialize the onboard OLED screen my B...

CMcD12 by Associate II
  • 893 Views
  • 0 replies
  • 0 kudos

How to get stable current consumption in sleep?

We are using STM32WB55RE in our application. we are trying to achieve ~10uA current consumption in sleep. But, 22uA(stable for 10min) immediately after entering sleep. After 10min current consumption start decreasing eventually to 14uA in next 60min....

vpaka.1 by Associate II
  • 2675 Views
  • 4 replies
  • 0 kudos

How to export STM32 project in STM32CubeIDE ?

I have used UART example code for P-NUCLEO_WB55 board to check it's UART.Now i want to share that project to another team memberBut if i just Copy paste project folder to other file location than it gives me compilation errors of Few files missing.I ...

JMeht by Associate
  • 6609 Views
  • 3 replies
  • 0 kudos

nucleo-WB55RG board BLE configuration

I am using the nucleo-WB55RG board. The problem is that it's my first time using BLE, but I don't know how to configure it to use Bluetooth as an advertising mode. I've seen a lot of data, but I don't know. Please tell me...

ckim.1 by Associate
  • 2019 Views
  • 1 replies
  • 0 kudos

How to correctly regenerate the LoRaWAN_End_Node.ioc code

hello,I am using a NUCLEO-WL55JCX and I have been using the LoRaWAN_End_Node application found within the STM32Cube_FW_WL_V1.3.0 package.I would like to use the ioc file to generate a clean project and then develop a custom application.I read the rea...

JTLGE by Associate II
  • 4093 Views
  • 5 replies
  • 0 kudos

Openthread SRP/DNS/mDNS problem

Hi Guys,I'm working with a P-NUCLEO-WB55 traying to implement an OpenThread network. I'm using the latest stable software package (1.15.0) with STMCubeIDE.I found some problem browsing response from the otDnsClientBrowse function. In particular, in t...

STM32WB, when atof() or strtod() BLE advertisement stops

I currently need a simple string to double/float function. For this I use atof() or strtod(). However whenever I call these functions the BLE advertisement stops and I cannot further connect to the WB.Does someone have the same problem?

YGail.2 by Associate III
  • 2903 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.