2023-02-07 2:28 AM
hello,
I am using a NUCLEO-WL55JCX and I have been using the LoRaWAN_End_Node application found within the STM32Cube_FW_WL_V1.3.0 package.
I would like to use the ioc file to generate a clean project and then develop a custom application.
I read the readme file but it did not help me, after copying in a diectory the ioc file I open it and it creates me a project that on stm32cube is not possible to open.
What are the steps I can take to handle the project properly?
2023-02-07 5:48 AM
In STM32CubeIDE -> File -> New -> STM32 Project From an existing STM32CubeMX Configuration File.
And you will be able to create a new project with .ioc File
2023-02-07 6:26 AM
thanks for the answer,
i tried to perform the steps you told me and now it creates my project on stm32 cube ide but when i go to compile it i have the following error :
In file included from ../LoRaWAN/Target/radio_conf.h:30,
from C:/Users/jacop/STM32Cube/Repository/STM32Cube_FW_WL_V1.3.0/Middlewares/Third_Party/SubGHz_Phy/stm32_radio_driver/radio_driver.h:45,
from C:/Users/jacop/STM32Cube/Repository/STM32Cube_FW_WL_V1.3.0/Middlewares/Third_Party/SubGHz_Phy/stm32_radio_driver/radio_driver.c:34:
../Core/Inc/platform.h:45:10: fatal error: stm32wlxx_nucleo_radio.h: No such file or directory
45 | #include "stm32wlxx_nucleo_radio.h"
| ^~~~~~~~~~~~~~~~~~~~~~~~~~
compilation terminated.
make: *** [Middlewares/SubGHz_Phy/subdir.mk:27: Middlewares/SubGHz_Phy/radio_driver.o] Error 1
make: *** Waiting for unfinished jobs....
In file included from ../LoRaWAN/Target/radio_conf.h:30,
from C:/Users/jacop/STM32Cube/Repository/STM32Cube_FW_WL_V1.3.0/Middlewares/Third_Party/SubGHz_Phy/stm32_radio_driver/radio_driver.h:45,
from C:/Users/jacop/STM32Cube/Repository/STM32Cube_FW_WL_V1.3.0/Middlewares/Third_Party/SubGHz_Phy/stm32_radio_driver/wl_lr_fhss.h:44,
from C:/Users/jacop/STM32Cube/Repository/STM32Cube_FW_WL_V1.3.0/Middlewares/Third_Party/SubGHz_Phy/stm32_radio_driver/radio.c:36:
../Core/Inc/platform.h:45:10: fatal error: stm32wlxx_nucleo_radio.h: No such file or directory
45 | #include "stm32wlxx_nucleo_radio.h"
| ^~~~~~~~~~~~~~~~~~~~~~~~~~
compilation terminated.
make: *** [Middlewares/SubGHz_Phy/subdir.mk:25: Middlewares/SubGHz_Phy/radio.o] Error 1
In file included from ../LoRaWAN/Target/radio_conf.h:30,
from C:/Users/jacop/STM32Cube/Repository/STM32Cube_FW_WL_V1.3.0/Middlewares/Third_Party/SubGHz_Phy/stm32_radio_driver/radio_fw.c:23:
../Core/Inc/platform.h:45:10: fatal error: stm32wlxx_nucleo_radio.h: No such file or directory
45 | #include "stm32wlxx_nucleo_radio.h"
| ^~~~~~~~~~~~~~~~~~~~~~~~~~
compilation terminated.
make: *** [Middlewares/SubGHz_Phy/subdir.mk:29: Middlewares/SubGHz_Phy/radio_fw.o] Error 1
"make -j4 all" terminated with exit code 2. Build might be incomplete.
15:21:51 Build Failed. 7 errors, 0 warnings. (took 1s.827ms)
2023-02-07 6:37 AM
To be confirm, but you need to import this file if you want to. This file is in BSP Folder. BSP folder link to your design board/custom board or nucelo board. If you try to do a new project on nucleo board. Then you can copy and add to your new project.
2023-02-07 6:49 AM
thanks again,
I found the BSP folder that is in the original examples folder.
how can i now put this folder inside the project and compile correctly? just copy it in there or do i also have to put the path in there somehow?
2023-02-27 3:19 AM
I imported the BSP folder by going to include the path in poject - properties - tool settings - MCU GNU COMPILER - include pats.
After adding this I get new errors:
c:\st\stm32cubeide_1.10.1\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.100.202210260954\tools\arm-none-eabi\bin\ld.exe: ./Application/User/LoRaWAN/Target/radio_board_if.o: in function `RBI_Init':
C:/Users/jacop/Desktop/test_stm32/LoRaWAN/Target/radio_board_if.c:74: undefined reference to `BSP_RADIO_Init'
c:\st\stm32cubeide_1.10.1\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.100.202210260954\tools\arm-none-eabi\bin\ld.exe: ./Application/User/LoRaWAN/Target/radio_board_if.o: in function `RBI_ConfigRFSwitch':
C:/Users/jacop/Desktop/test_stm32/LoRaWAN/Target/radio_board_if.c:127: undefined reference to `BSP_RADIO_ConfigRFSwitch'
c:\st\stm32cubeide_1.10.1\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.100.202210260954\tools\arm-none-eabi\bin\ld.exe: ./Application/User/LoRaWAN/Target/radio_board_if.o: in function `RBI_GetTxConfig':
C:/Users/jacop/Desktop/test_stm32/LoRaWAN/Target/radio_board_if.c:153: undefined reference to `BSP_RADIO_GetTxConfig'
c:\st\stm32cubeide_1.10.1\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.100.202210260954\tools\arm-none-eabi\bin\ld.exe: ./Application/User/LoRaWAN/Target/radio_board_if.o: in function `RBI_IsTCXO':
C:/Users/jacop/Desktop/test_stm32/LoRaWAN/Target/radio_board_if.c:179: undefined reference to `BSP_RADIO_IsTCXO'
c:\st\stm32cubeide_1.10.1\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.100.202210260954\tools\arm-none-eabi\bin\ld.exe: ./Application/User/LoRaWAN/Target/radio_board_if.o: in function `RBI_IsDCDC':
C:/Users/jacop/Desktop/test_stm32/LoRaWAN/Target/radio_board_if.c:205: undefined reference to `BSP_RADIO_IsDCDC'
c:\st\stm32cubeide_1.10.1\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.100.202210260954\tools\arm-none-eabi\bin\ld.exe: ./Application/User/LoRaWAN/Target/radio_board_if.o: in function `RBI_GetRFOMaxPowerConfig':
C:/Users/jacop/Desktop/test_stm32/LoRaWAN/Target/radio_board_if.c:231: undefined reference to `BSP_RADIO_GetRFOMaxPowerConfig'
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.