STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

How can i use IOC from example project in new project?

I have a STM32WLC1 board with 2 processors. I would like to develop a LoRa based Project that uses both cores. However the example code of Lorawan-Endnode found here:[link removed because newest members cannot add links]uses only one core and has an ...

AFast.1 by Associate
  • 1387 Views
  • 2 replies
  • 0 kudos

Resolved! Code generation problem for RTC with STM32WL

I'm currently having problems with the code generated by CubeMx for the RTC on my STM32WL MCU. Indeed, after generating the code and building the project, there are errors in the timer_if.c file. Each time the rtc handler is used, it says that the re...

MLour.1 by Associate
  • 4184 Views
  • 5 replies
  • 1 kudos

xbee with stm32 little question

I am doing xbee communication with stm32, I am sending and receiving data, there is no problem, but I cannot see message on the serail monitor of stm32. (but it appears in debug process) why?

Loodan22 by Associate II
  • 1876 Views
  • 2 replies
  • 0 kudos

Resolved! BLE and LLD at the same time

Hello,Is it possible to work with one STM32WB central role as router in BLE and in LLD mode?As router I mean communicate in BLE to one smartphone and communicate in LLD with several remotes.The issue is that the CM0 coprocessor firmware is different ...

PCu1 by Senior
  • 1594 Views
  • 2 replies
  • 0 kudos

Verification of Crystal suitability for STM32WL design

We have a design implementing the STM32WL55/WE5.The recommended crystals on the reference designs and literature are:NX2012SA 32.768KHz EXS00A-MU00527X2NX2016SA 32MHz EXS00A-CS06465I want to verify that it is OK to use the following:For NX2016SA:  EI...

DRoss.3 by Associate
  • 2776 Views
  • 1 replies
  • 0 kudos

Resolved! STEVAL-Proteus (STM32WB55MMG): Custom BLE application

Hello,I am trying to design a BLE custom template application. I start by following the STM32WB Bluetooth® LE - STM32CubeMX Application Conception (https://wiki.st.com/stm32mcu/wiki/Connectivity:STM32WB_BLE_STM32CubeMX) using the P-NUCLEO-WB55 board ...

0693W00000aHPSSQA4.png 0693W00000aHPT6QAO.png
ALABR.1 by ST Employee
  • 2570 Views
  • 1 replies
  • 1 kudos

Resolved! How to use aci_gatt_add_char_desc() for STM32WB BLE?

My biggest issue currently is on my external app which is connecting to the WB that it cannot get the descriptor.As I debug using BLE using LightBlue there is no descriptor in my characteristic. As I notice recently by reading again the manual there ...

0693W00000aH1FKQA0.jpg
YGail.2 by Associate III
  • 2544 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.