2023-03-28 6:15 AM
Hello,
to get a lower power consumption in my application i would like to go in stop mode 2 and wake up shortly to receive some characters on the LPUART.
But unfortunately my mcu does not wake up. I can see with the debugger that the send Byte is in the DR of the LPUART and after leaving the stop mode I also end up in the LPUART_ISR.
It seems to me that I forget something or do something wrong. Therefore I am looking for help here.
Currently I set the following registers before entering stop mode 2
in LPUART1->CR1 USART_CR1_UESM
in LPUART1->CR3 USART_CR3_WUFIE
in LPUART1->ICR USART_CR3_WUCF
LSE is running and propagated and selected for LPART1 by 9600 Baud
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.