2023-04-25 4:26 AM
Hey!!
I have a BLE application which runs on custom server profile. There are few characteristics of a given service, where the client can modify them. I need clarifications for the below questions.
Thanks,
Akash
2023-04-26 4:57 AM
@Remy ISSALYS @Remi QUINTIN
Can you guys please help me out with this??
2023-04-26 6:43 AM
Hello,
You can refer to AN5270 which describes all the commands and the events available.
• Write without response
• Signed write without response
• Write characteristic value
• Write long characteristic value - reliable write
Best Regards
2023-04-26 11:29 PM
@Remy ISSALYS ,
Based on your inputs, I looked out for the HCI_LE_CONNECTION_COMPLETE_SUBEVT_CODE event. This event is handled in the 'SVCCTL_App_Notification' function. I had a break-point here, when the connection was made, this break-point was not hit.
Also, similar thing happened with the attribute modified value event which is handled in 'Custom_STM_Event_Handler' . The break-points I had did not hit.
The application is running on FreeRTOS. The shci_user_evt_proc(); is not called getting called after the BLE Init
2023-04-27 1:20 AM
Hello,
Can you describe what you want to do? Which board are you using? Is it in front of a smartphone or another board? And can you describe your use case?
Best Regards
2023-04-27 2:20 AM
Hey @Remy ISSALYS ,
2023-04-28 9:50 AM
Hello,
Try to remove the optimization in your project, you should receive the HCI_LE_CONNECTION_COMPLETE_SUBEVT_CODE event when the connection occurred unless you are using privacy or extended advertising, in the case you will receive the HCI_LE_ENHANCED_CONNECTION_COMPLETE_EVENT event.
Best Regards
2023-05-01 11:21 PM
Hey @Remy ISSALYS,
The optimization levels are set to None(-O0). And I'm not using the privacy/extended advertising.
2023-05-02 11:05 PM
@Remy ISSALYS ,
Hello, the issue got resolved btw. This was due to not allocating enough heap memory in the IOC.
Can you suggest the minimum required heap for the BLE applications?
Thanks,
Akash
2023-05-04 9:13 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.