STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

BLE advertisement with irregular time intervals

Hi,We are testing BLE advertisement intervals in noisy environment(where there are multiple BLE devices around). The minimum and maximum BLE advertisement intervals we set are 20ms and 40ms. Usually when we place the device in shielded box all the ad...

_legacyfs_online_stmicro_images_0693W00000bkuxiQAA.png
vpaka.1 by Associate II
  • 1560 Views
  • 0 replies
  • 0 kudos

I have to unplug Nucleo after flash to start BLE stack.

Whenever I upload code to my STM32 WB55 Nucleo to start Wireless stack (when I do not unplug and plug again there is no BLE device when I open ST BLE Toolbox) I have to manually reset device.Is there a way to skip that step? I mean, when I do debug i...

dnj by Associate III
  • 2424 Views
  • 3 replies
  • 1 kudos

Is it possible to power an STM32WLE5 with variable voltage ?

Hello,I would like to power an STM32WLE5 with two voltage levels:VBAT: 2 series AA batteries, yielding a voltage comprised between (~3.2V and ~2V) over the life of the batteries.VBOOST: A boosted voltage from the batteries with a target of 3V. If the...

ABrua.1 by Associate II
  • 1327 Views
  • 0 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.