2023-05-24 1:59 AM
Hello
I set the variable uint8_t test as test = test + 1 in main.c
and send this variable via BLE in p2p_server_app.c to PC with next command
P2PS_STM_App_Update_Char(P2P_NOTIFY_CHAR_UUID, (uint8_t *) (&local));
Also, set it in main.h extern uint8_t test
and include the header in both files main.c and p2p_server_app.c
But when I send this variable from the p2p_server_app via Bluetooth to PC it is sent stable value, not updated value every time. it seems to me that this STM32WB is dual-core and apparently each core works separately. it turns out I can consider changes for "test" only once, how can I make the p2p_server_app.c takes updated value from main.c
// main.h
extern uint8_t test;
// main.c
#include "main.h"
uint8_t test= 0;
while (1)
{
test = test + 1;
}
// p2p_server_app.c
#include "main.h"
P2PS_STM_App_Update_Char(P2P_NOTIFY_CHAR_UUID, (uint8_t *) (&local));
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.