2023-06-05 1:10 PM
I am developing an application on the Seeed Lora-E5 module, which contains an STM32WLE5.
Currently I am programming the device via the SWD interface, but for future firmware updates I want to use the UART, (this UART is available externally through a USB-UART chip).
The problem now is how to make the device switch to the internal bootloader : unfortunately the Boot0 (PH3) PIN on the STM32WLE5 is NOT made available on the package of the Seeed Lora-E5 module, so I cannot use that pin..
From the AN3155 I see that the CubeMx Programmer is sending 0x7F to the UART, in order for the MCU to select the UART as programming interface.
So here is my idea : after reset, I could listen to the UART for eg. 30 seconds, and if in this time a 0x7F byte arrives, jump to the bootloader. (if the 30 seconds expire, the device starts in normal operation mode).
I am aware that the bootloader expects the MCU in the same state as after reset, so I will take that into account, be resetting already configured UART (and other modified peripherals)
Does this make sense ? Any comments ? Did anyone try this ?
Thank you!
Solved! Go to Solution.
2023-06-07 4:57 AM
As I got no immediate response, I decided to try it out, and it actually works.
Here is some demo code :
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_USART2_UART_Init();
logging::detectDebugProbe();
logging::snprintf("normal boot...\n");
uint8_t data[1];
HAL_StatusTypeDef result;
while (1)
{
result = HAL_UART_Receive(&huart2, data, 1, 5);
if (result == HAL_OK)
{
if (data[0] == 0x7F)
{
logging::snprintf("jmp..\n");
HAL_UART_DeInit(&huart2);
JumpToBootloader();
}
}
}
}the body of
JumpToBootloader();can be found here :
How to jump to system bootloader from application code on STM32 microcontrollers
Mind the logging:: statements, this some SWO debug class I use to monitor what's going on. They are not needed for the mechanism to work.
2023-06-07 4:57 AM
As I got no immediate response, I decided to try it out, and it actually works.
Here is some demo code :
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_USART2_UART_Init();
logging::detectDebugProbe();
logging::snprintf("normal boot...\n");
uint8_t data[1];
HAL_StatusTypeDef result;
while (1)
{
result = HAL_UART_Receive(&huart2, data, 1, 5);
if (result == HAL_OK)
{
if (data[0] == 0x7F)
{
logging::snprintf("jmp..\n");
HAL_UART_DeInit(&huart2);
JumpToBootloader();
}
}
}
}the body of
JumpToBootloader();can be found here :
How to jump to system bootloader from application code on STM32 microcontrollers
Mind the logging:: statements, this some SWO debug class I use to monitor what's going on. They are not needed for the mechanism to work.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.