STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

STM32WB55 > GFSK module access

Dear Community,We do an update on a old product and the goal is to replace the nRF52840 by the STM32WB55.The STM32WB datasheet is clear about BLE capacity but i would to know if we can use it without the Bluetotth stack, with my own protocol as we do...

JL_Loyd by Associate II
  • 1922 Views
  • 1 replies
  • 0 kudos

STM32WB55

STM32WB55 UpdateCharacteristic size.Hello, I'm using the STM32WB55 on the NUCLEO Board.I need to change the Char_Value_Length in the same connection. For example, the first UpdateCharacteristic size = 50Byte and after change to 55 Byte.It is possibl...

Prisma by Associate II
  • 855 Views
  • 0 replies
  • 0 kudos

Debug mode terminating after Radio.Rx() func. called

hello everyone, I am currently working on a board that I designed based on the double-layer reference design of MB1874-LP. The board is almost identical to the reference design.After finishing the layout of the board, I uploaded the draft code I wrot...

mrkayaalp_2-1690235543347.png mrkayaalp_3-1690235581996.png mrkayaalp_4-1690235664202.png
mrkayaalp by Associate III
  • 1653 Views
  • 1 replies
  • 0 kudos

BLE Mesh Static Net- and App-Key

Hi, I have STM32WB55RG Board and I have tried the BLE Mesh Demo. I was wondering, it is possible to set the Net and App-Key with static value? If it is possible, then how to do it?I tried on 'BLE_MeshPRFNode' project.Thanks!

osugi_w by Associate
  • 1759 Views
  • 1 replies
  • 0 kudos

BLE questions related to WB55

Hello,The objective of the project is to develop a BLE custom server profile and I need some clarifications.The maximum number of characters AD_TYPE_COMPLETE_LOCAL_NAME_LENGTH for the complete name for advertisement is restricted to 11. Is there any ...

0693W00000WJywBQAT.png 0693W00000WJJcUQAX.png
ABN by Associate III
  • 3285 Views
  • 5 replies
  • 2 kudos

STM32WB55 power consumption

Hi,I have a board which has a STM32WB55RGV6 MCU and i have a problem. When i connected my board to Power supply, it consumes just 13 mA. But then suddenly, it increased 94 mA. I measured resistance between GND and VDD_MCU pins. I was 53 ohm. I unders...

Makif by Associate
  • 1481 Views
  • 1 replies
  • 0 kudos

Resolved! stm32WB Security standar

Hi!I've some doubts about security features of stm32WB.After reading the documentation, forums, etc; I can find that stm32WB implements all 4 security levels of Security Mode 1, which includes the ECDHE P-256 cryptography.I've some questions about th...

j.villar by Associate II
  • 2076 Views
  • 1 replies
  • 1 kudos

Random BLE connection fail on STM32WB

Hello all,We are developing a product that connects to a mobile application through BLE. Sometimes, not all the time, the product does not connect to the smartphone the first time, it retries to connect until it gets there. As a consequence, the conn...

audrey38_0-1689064299779.png
audrey38 by Associate II
  • 1789 Views
  • 1 replies
  • 0 kudos

STM32WB55 Read Notify Characteristic Event

Hello,Is there any way to catch ACI event dedicated to read NOTIFY characteristic?I tought about ACI_ATT_READ_RESP_EVENT event, but I'm not sure if it is correct if I use with notify Characeristic.Could you confirm me that is a good way to achieve wh...

dnj by Associate III
  • 1465 Views
  • 1 replies
  • 0 kudos

Purchaing 'Qualification Fee' for using BlueNRG module

Hi  I am planning to use the BlueNrg module in my project , until I found out that I have to pay for the Qualification fee for using BlueTooth. Not sure if I dont display the logo I dont have to purchase it, or do I have to purchase it even if the lo...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.