2023-07-04 2:25 AM - last edited on 2023-07-05 9:55 AM by Remy ISSALYS
Hi!
I've some doubts about security features of stm32WB.
After reading the documentation, forums, etc; I can find that stm32WB implements all 4 security levels of Security Mode 1, which includes the ECDHE P-256 cryptography.
I've some questions about that:
If I enable pairing with no fixed PIN selected, Display Only I/O Capability and MITM protection requierd bit enabled, could I asume that after pairing process with the device, the communication will be encrypted? If so, which encryption would be established, AES-CMAC, ECDHE P-256, both or none?
I've already been able to program the stm32wb to advertise data, print PIN from terminal and pairing my phone to the stm32WB, but I would like to know if that is all, or if I need more steps to encrypt communications.
Thank you in advance!!
Solved! Go to Solution.
2023-07-27 9:17 AM
Hello,
It depends to the value of CFG_SC_SUPPORT parameter in app_conf.h file in your application, see below:
/**
* Define Secure Connections Support
*/
#define CFG_SECURE_NOT_SUPPORTED (0x00)
#define CFG_SECURE_OPTIONAL (0x01)
#define CFG_SECURE_MANDATORY (0x02)
#define CFG_SC_SUPPORT CFG_SECURE_MANDATORY
If it's set to CFG_SECURE_NOT_SUPPORTED, it means the LE Legacy pairing will be used.
If it's set to CFG_SECURE_OPTIONAL, LE Legacy pairing or LE Secure Connections will be used depending of the peer device supported feature.
If it's set to CFG_SECURE_MANDATORY, it means the LE Secure Connections will be used.
The LE Legacy pairing is based on AES-CCM encryption and the LE Secure Connections is based on FIPS-approved algorithms (AES-CMAC and P-256 elliptic curve).
Best Regards
2023-07-27 9:17 AM
Hello,
It depends to the value of CFG_SC_SUPPORT parameter in app_conf.h file in your application, see below:
/**
* Define Secure Connections Support
*/
#define CFG_SECURE_NOT_SUPPORTED (0x00)
#define CFG_SECURE_OPTIONAL (0x01)
#define CFG_SECURE_MANDATORY (0x02)
#define CFG_SC_SUPPORT CFG_SECURE_MANDATORY
If it's set to CFG_SECURE_NOT_SUPPORTED, it means the LE Legacy pairing will be used.
If it's set to CFG_SECURE_OPTIONAL, LE Legacy pairing or LE Secure Connections will be used depending of the peer device supported feature.
If it's set to CFG_SECURE_MANDATORY, it means the LE Secure Connections will be used.
The LE Legacy pairing is based on AES-CCM encryption and the LE Secure Connections is based on FIPS-approved algorithms (AES-CMAC and P-256 elliptic curve).
Best Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.