STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4119 Views
  • 0 replies
  • 3 kudos

P-Nucleo-WB55 and X-Nucleo-DRP1M1 compatibility

Hi all. The documentation of DRP1M1 says it can be stacked on top any Nucleo board with UCPD peripheral embedded in their microcontrollers. I don't see UCPD feature in WB55RG so I thought they are not compatible. However, my supplier is positive that...

Nos by Associate
  • 1982 Views
  • 1 replies
  • 0 kudos

STM32WL error flashing with enabled LoRa middleware

Hello everyone,I have an Olimex BB-SMT32WL that is based on a STM32WLE5CCU6. I use STM32CubeIDE and opened a new project for exactly the STM32WLE5CCU6.Firmware Package Name and Version STM32Cube FW_WL V1.3.0If I just configure like a GPIO Output to H...

Resolved! How to get out from the BLE Function or How to turn off BLE.

Hi hope you guys are well,  When i call the function to turn the BLE on, it starts to advertise but i dont know to get out of that function , means in the main while loop the code is stuck at MX_APPE_Proccess(), i did the debugging but its just loopi...

URGENT: STM32WLE5 custom design questions

I have a fast track project for which I need to do a quick feasibility study, determine if STM32WL is suitable candidate, and if so, have enough support available to design it in. So all your timely, insightful help would be greatly appreciated. Here...

AVigh.1 by Associate II
  • 16487 Views
  • 9 replies
  • 0 kudos

STM32WL problems with sending data. SOLVED.

Hi!EDIT 4: it was solved, and the solution at the end of the post.I did a hardware design based on the STM32WL55 chip + Balun and one line for controlling the radio, FE_CTRL1. I modified the HAL radio library for all the SET-RESET only using RF_SW_CT...

RobMBSos_0-1697482106536.jpeg RobMBSos_1-1697482173421.jpeg RobMBSos_2-1697482182152.jpeg RobMBSos_0-1697481026898.png
RobMBSos by Associate
  • 3335 Views
  • 0 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.