2023-05-22 10:30 PM - last edited on 2023-11-30 7:07 AM by Amel NASRI
Hi all.
The documentation of DRP1M1 says it can be stacked on top any Nucleo board with UCPD peripheral embedded in their microcontrollers. I don't see UCPD feature in WB55RG so I thought they are not compatible.
However, my supplier is positive that the X-Nucleo-DRP1M1 can be used with P-Nucleo-WB55 so I get a little confused here. In the end, can I use the X-Nucleo-DRP1M1 with the P-Nucleo-WB55?
Thank you.
2023-10-17 8:53 AM
Hi Nos,
To use X-NUCLEO-DRP1M1 with TCPP03-M20 in order to perform a Dual Role Port application, the STM32 must embed UCPD controller.
Unfortunately, STM32WB55 series do not embed this controller. I've performed the check using Cube-MX.
Fortunatly, 685 others STM32 embeds UCPD. I hope, you will find the one that corresponds to your needs.
Or, if only type-C SINK or SOURCE limited to 5V - 3A, you can use TCPP01-M12 or TCPP02-M18 and use associated X-NUCLEO-SNK1 or X-NUCLEO-SRC1. Then, resources must be attributed according to the examples on X-CUBE-TCPP.
Best regards,
Mathieu
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.