2023-10-16 4:11 AM
Hello everyone,
I have an Olimex BB-SMT32WL that is based on a STM32WLE5CCU6. I use STM32CubeIDE and opened a new project for exactly the STM32WLE5CCU6.
Firmware Package Name and Version STM32Cube FW_WL V1.3.0
If I just configure like a GPIO Output to High it compiles and I can succesfully flash and debug it using STM32CubeIDE and openocd gdb running via terminal.
But as soon as I open the .ioc and simply enable SubGHZ and LoRaWAN things stop working, while it still compiles it won't flash anymore, throwing me this error:
(I also tried Arduino STM32duino but I'm getting the same error..)
Open On-Chip Debugger 0.12.0-00024-gc3ff39f8b (2023-06-26-16:51) [https://github.com/STMicroelectronics/OpenOCD]
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
swd
adapter speed: 1000 kHz
stm32wlx_cti_prepare_restart_one
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : CMSIS-DAP: SWD supported
Info : CMSIS-DAP: FW Version = 1.0
Info : CMSIS-DAP: Interface Initialised (SWD)
Info : SWCLK/TCK = 1 SWDIO/TMS = 1 TDI = 0 TDO = 0 nTRST = 0 nRESET = 1
Info : CMSIS-DAP: Interface ready
Info : clock speed 4000 kHz
Info : SWD DPIDR 0x6ba02477
Info : [stm32wlx.cm4] Cortex-M4 r0p1 processor detected
Info : [stm32wlx.cm4] target has 6 breakpoints, 4 watchpoints
Info : starting gdb server for stm32wlx.cm4 on 3333
Info : Listening on port 3333 for gdb connections
Info : accepting 'gdb' connection on tcp/3333
Info : device idcode = 0x10016497 (STM32WLE/WL5x - Rev 'unknown' : 0x1001)
Info : RDP level 0 (0xAA)
Info : flash size = 256 KiB
Info : flash mode : single-bank
undefined debug reason 8 - target needs reset
[stm32wlx.cm4] halted due to debug-request, current mode: Thread
xPSR: 0x01000000 pc: 0x1fff2b6c msp: 0x20001508
Info : Padding image section 0 at 0x0800f894 with 4 bytes (bank write end alignment)
Info : SWD DPIDR 0x6ba02477
Error: Failed to write memory at 0x20009ff8
Error: block write failed
Error: error writing to flash at address 0x08000000 at offset 0x00000000
Warn : keep_alive() was not invoked in the 1000 ms timelimit. GDB alive packet not sent! (6795 ms). Workaround: increase "set remotetimeout" in GDB
[stm32wlx.cm4] halted due to debug-request, current mode: Thread
xPSR: 0x01000000 pc: 0x1fff2b6c msp: 0x20001508
shutdown command invoked
Info : dropped 'gdb' connection
Thanks in advance
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.