STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Need 2-layer reference design for 433MHz LoRa

Hello, the reference design STDES-WL5U2SBB (MB1791) specifies a frequency range between 470-530 MHz. I plan to run LoRa on 433MHz with 10 dBm. I do not wish to use a 4-layer PCB in my product design. This seems to be the only version that has 2-layer...

Resolved! Porting STM32CubeWB code from WB55 to WB15 board

In the STM32CubeWB source code collection, I found the BLE_Peripheral_Lite project. This project however is only available for the P-NUCLEO-WB55, but I am working with the NUCLEO-WB15 board.According the Release notes this should be easy:<quote>The p...

_Ben by Associate
  • 2151 Views
  • 2 replies
  • 1 kudos

How to inspect the clock source for RTC?

I have three STM32WB55 applications:A) is a debugging application that's only ever flashed directly and standalone using the STM32CubeProgrammer CLI.B) is a bootloader with integrated FUOTA functionality.C) is my "actual" application. It can be compi...

LWChris_0-1698758968761.png LWChris_1-1698759000772.png
LWChris by Associate III
  • 8202 Views
  • 8 replies
  • 0 kudos

Power Consumption Help with STM32wb55

Hello -    I have a custom pcb using the stm32wb55 and I have spending time optimizing the power consumption. My primary intentions with this PCB is to sample data around 1 Hz and send this data to html server app using BLE. I'm using the BLE_Sensor ...

od805_0-1701307125467.png od805_1-1701307167318.png
od805 by Associate III
  • 6253 Views
  • 4 replies
  • 1 kudos

Implementing firmware update over the air (OTA) on STM32WB

Hello everyone,I'm working on a project which includes the following hardware setup.> Raspberry Pi 4 Model B> STM32WB55RGV6 Nucleo board> WizNet W5500 Ethernet Module I'm using SPI protocol to communicate between STM32WB board and WizNet W5500 module...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.