STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Save energy with CPU2 in iddle mode on STM32WB10

I am a new developer on STM32WB10 and I do not succeed to  drastically decrease power consumption in standby mode. Commands for main CPU in order to lower consumption seems to be OK but the CPU2 for BLE seems to be always active.LL_C2_PWR_SetPowerMod...

Resolved! Replacing power inductors in NUCLEO-WL5JC MB1389 schematics

Hello everyone,I'm seeking your guidance regarding the substitution of 0402 inductors with 0603 in the NUCLEO-WL5JC MB1389 high band schematics (https://www.st.com/resource/en/schematic_pack/mb1389-wl55jc-highband-e02_schematic.pdf). In the RF sectio...

Levan_0-1704277640913.png
Levan by Associate III
  • 4692 Views
  • 2 replies
  • 1 kudos

LBAD0XX1SC-DM interface with STM32WB55RE

Hello,I am using STM32WB55RW (MCU) +  muRata module(LBAD0XX1SC-DM) in my custom HW.X-CUBE-CELLULAR expansion package is available for STM32Cube but its contain example project for L4  series (STM32L462REY6TR).Can you please share sample code if anyon...

I have loaded the example ZigBee_OnOff_server_coord into Nucleo board. I have also loaded "stm32wb5x_Zigbee_FFD_fw.bin" rf stack. My FUS version is 1.12.0 .

When I run the application, all three LEDs are toggling in cyclic fashion and according to the note, this is an error condition. I checked the message from serial port and I am getting the following[0m[M4 APPLICATION] WIRELESS COPROCESSOR FW:[0m[M4 A...

BLE Not starting after power-up

Hi,I'm having an error after powering the MCU, it looks like the CPU2 with the BLE stack it's not restarting.The error occurs when I stop advertising, the BLE status is APP_BLE_IDLE and I turn off the board.When I power-up the board and do the BLE in...

Pablo1610 by Associate II
  • 1666 Views
  • 1 replies
  • 0 kudos

Resolved! Zigbee: ip802154_lld_exitSleep() FAILED

Hello, testing Zigbee_OnOff_Client_SED on P-NUCLEO-WB55. Sources are from version 1.18.0, same as installed stm32wb5x_Zigbee_FFD_fw.bin. Almost no changes to source files except modification channelmask to WPAN_CHANNELMASK_2400MHZ.After a while (rand...

SToma by Associate III
  • 6593 Views
  • 7 replies
  • 1 kudos

Communication through Lora with STM32L0

Hello, I would like you to help me to communicate two microcontrollers (The B-L072Z-LRWAN1 Discovery kit LoRa/Sigfox module (Murata) using Lorawan, I was researching and looking at some libraries that were an expansion for Lorawan. But I don't know h...

MVega.1 by Associate
  • 2469 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.