STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Wireless M-Bus (wMbus) and LoRaWAN

Hello,We are in the process of developing a smart meter that will feature dual communication capabilities supporting both Wireless M-Bus (wMbus) and LoRaWAN. Our aim is to use a single chip for this purpose, with the advantage of sharing the same ant...

Resolved! STM32WB How to use GATT caching?

Hello,I'm using BLE_p2pClient and BLE_p2pServer programs.I had pairing request in BLE_p2pClient to have both devices bonded.Now, I want to have a fast connection between client and server; actually, the connection between client and server is about 2...

FWX by Associate III
  • 3296 Views
  • 5 replies
  • 0 kudos

Resolved! X-CUBE-BLE1 SampleApp: How it works ?

Hi ST Community,I'm using the B-L475E-IOT01 card and I want to use the X-CUBE-BLE1 middleware to send information directly to a variable (something I was thinking of doing simply with this application). Only, when I run it and try to debug, I'm havin...

FUS running but not able to load Stack?

I am trying to load the p2p server example and noticed my Nucleo-WB15CC doesn't do any bluetooth communication. I can run normal user code just fine (LEDs, GPIO etc.) but CPU2 doesn't seem to do anything.When I try to start FUS, I get this:When I try...

tester_1-1691183454986.png tester_0-1691183405200.png
tester by Associate III
  • 5607 Views
  • 8 replies
  • 0 kudos

how to do an operation on specific BLE link

ACI_HAL_GET_LINK_STATUS will give an Array of link status (eight links).My question is how do I do operations on specific links of my choice?e.g., start an advertisement on a specific link. reference AN5270 -  

DS4_0-1705176521476.png
DS.4 by Senior II
  • 1671 Views
  • 2 replies
  • 1 kudos

Resolved! STM32F411 as basis platform with STM32WB1MMC

(1) Are there any experience for a data exchange via bluetooth between two STM32WB1MMC-parts? (2) How can I use a STM32WB1MMC together with a STM32F411 board? Are there any experiences? (3) How can I create a data exchange between two STM32WB1MMC? (4...

timbo2023 by Associate III
  • 2389 Views
  • 3 replies
  • 0 kudos

Resolved! STM32WB5MM-DK, Zigbee_OnOff_Client_Router, FATAL ERROR

Hello,I have STM32WB5MM-DK evaluation kit and I am trying to get example Zigbee_OnOff_Client_Router working. I updated FUS (v. 1.2.0) and Zigbee FFD (v.1.18.0). Example do not work, I get an error "Fatal Error" on terminal and display:[M4 APPLICATION...

eskomj by Associate III
  • 4660 Views
  • 7 replies
  • 0 kudos

STM32WB55 unresponsive Wireless Stack

I have a problem with my wireless stack which was fixed by unplugging and pluggin back in my NUCLEO-WB55. Everything was working well for many months, but I recently tried downloading the ST example project BLE_DataThroughput (from the STM32Cube_FW_W...

SA1 by Associate
  • 1717 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.