NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello STM32 Community,I hope this message finds you well. I am currently working on a project that involves integrating Bluetooth Low Energy (BLE) communication into an STM32CubeIDE project. Specifically, I am facing a challenge in reading the update...
I attendded a trainning last year on STM32WL5M, we were told this product will be available 2024 January. I have been checking but looks like is not available.Do anyone have information when this product will be available?
Hello,In a Client(Router)/Server configuration with two STM32WB55 I would like to accelerate the transmission of data at starting of the server.The server address is know in advance and stored in the client then in the HCI_LE_ADVERTISING_REPORT_SUBEV...
I work with the STM32WB5MMG (bluetooth Low Enenrgy 5.0 and 802.15.4 module).I can’t find any documentation regarding the allocation of each pin of the chip.the datasheet I found indicate a type I/O and a reference of the type "PB10" or "PD2".... but ...
Hi all, I am experiencing a problem with the DMA of the STM32WBA52 (on the NUCLEO-WBA52CG board) when using it to transfer data from FLASH to USART1 TX : part of the transmitted data is modified, i.e. not the data that is found in FLASH)The problem o...
Hello,How should I make connection to the Tuya gateway with zigbee? I have read zigbee wiki dokumentation about zigbee binding. I have understand that I should use "find and bind" mechanism in that case. I tried to find suitable example from github, ...
Hello fellow developers,I'm currently working on a project using the STM32WL board and a LoRa application. I've encountered an issue with the RTC (Real-Time Clock) that's perplexing me, and I hope someone can shed some light on it.In my project, I'm ...
Hi,I'm trying to use usb device of my STM32WB55RG Nucleo board but when I connect my device to computer, I got a "USB Device not recognized" error. I used "LL_HSEM_1StepLock( HSEM, 5 )" function before APPE init. How can i get rid of this error?Best ...
Greetings,Can I replace NX3L1T3157GM analog switches on en.MB1389-WL55JC-highband-E02_Schematic with FSA5157L6X ?Thanks in advance
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.