STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! Fixed_Pin change between connections

Curious regarding using ACI_GAP_SET_AUTHENTICATION_REQUIREMENT to change the fixed pin after already using a different pin key for a previous connection. Would that work? Any bad consequences?

DS.4 by Senior II
  • 1946 Views
  • 2 replies
  • 2 kudos

STM32WL33

Hi can MCU STM32WL33 - QFN32 work with the balun BALF-SPI-01D3? Where can I find the solution on 2-layer PCB (for 868MHz)? // for Antenna johanson 0868AT43.. regards zbyno

zbynoB by Associate II
  • 1062 Views
  • 0 replies
  • 0 kudos

BLE Eddystone BlueNRG2 read Characteristic on firmware

Hello community, I am trying to read a characteristic before each advertisement on BlueNRG-2 devboard.   I started from the example BLE_Sensor_Demo, I adapted the services and characteristics. I want to use a characteristic as a flag. When characteri...

Resolved! STM32WB: Thread network goes down after a few minutes in BLE Thread Dynamic Mode but BLE stays active and works fine.

I created a custom application using the code from the BLE_THREAD_DYN example and the v10.0 FW BLE_THREAD_DYN stack. The BLE works fine but the thread stack goes down after a few minutes. The main differences between my code and the example is that I...

Resolved! STM32WB55 RTC with battery backup

Hello everyone, I hope you are well.I'm working with the STM32WB55. I'm having difficulty getting RTC to work correctly.The VBat is always powered by 3v3, I have an on/off switch that only removes the power from the VDD, however, when I turn it off a...

ffjunq by Associate III
  • 3248 Views
  • 4 replies
  • 0 kudos

Amazon Sidewalk Support for STM32WL

Currently, there isn't any support for Amazon Sidewalk for the STM32WL. The only supported vendors are Nordic, Silicon Labs, Texas Instruments, and Quectel. Reading through the AWS Sidewalk spec, it seems like the chip could support it in CSS and FSK...

DWalk.3 by Associate III
  • 2949 Views
  • 3 replies
  • 3 kudos

Resolved! RTC is not incremented with a voltage Vbat below 0.6V

Hello,we use an STM32WB55 with an RTC backup via a super capa.when the Vbat voltage drops below 0.6V, the RTC registers are no longer incremented.if the board reboots at this point, we have a datetime offset.is it possible to detect this problem when...

Resolved! Using OLED and gyroscope of STM32WB5MM-DK

I am using STMcube ide for developing applications with STM32WB5MM-DK. I will be trying to use the OLED display and gyroscope of the discovery board. I couldn't find suitable tutorial or documents for accessing. Is there any documents available for t...

Manually sending an I2C stop command.

In the manual it says that a stop command will be sent with the next byte if the CR2 stop flag is high.  Is there a way to send a stop command immediately rather than with the next byte?  I'm asking because I have a section of code where I send a sta...

Jcoll1_0-1707080808253.png
Jcoll.1 by Associate III
  • 5510 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.