STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4119 Views
  • 0 replies
  • 3 kudos

Resolved! STM32L0 LoRaWAN -> Whenever I set date and time to internal RTC, my system will crash.

Hello,I'm currently working with an STM32 microcontroller, and I'm facing a challenge related to the internal Real-Time Clock (RTC). Specifically, whenever I attempt to set the date and time using the internal RTC, my system crashes. I've reviewed th...

Resolved! Multitasking radio and sensor reading task.

Hello, I am currently building an application for the STM32WL. Two processes need to run simultaneously, the first is offline, and just reads data from a sensor and stores it in SD memory. The second is sending a LoRaWAN up-link message every 10 minu...

jflaxman by Associate II
  • 4623 Views
  • 3 replies
  • 0 kudos

Fail to find my nucleo-WL55JC2 in the BLE Sensor App

Hello everyone, So I'm following the tutorial here https://www.st.com/en/embedded-software/x-cube-ble2.html to try a BLE connection from the nucleo-WL55JC2 connected to the BLE expansion board X-NUCLEO-BNRG2A1. I followed the tutorial and run the pro...

LearnCORE by Associate II
  • 4108 Views
  • 4 replies
  • 0 kudos

Resolved! Can't download STSW-BNRG2N-V320 Package

Hello, I tried many times(with different browsers) to download the package to use it with the BLE-NRG2-Module(Evaluation-Board). The Page keeps looping between login and the main-page with no success.     Thank you Amir

AElgh by Associate III
  • 2375 Views
  • 3 replies
  • 0 kudos

Resolved! UTIL_SEQ_WaitEvt and HW timer

Hi I have a infinite loop that wait an event set in a gpio interrupt bywhile(1){UTIL_SEQ_WaitEvt()...}It works.Now, I want have a timer after this so, if the interrupt doen't fire for some second, I want to exec a callback function.I added after UTIL...

AColl.7 by Associate II
  • 2067 Views
  • 2 replies
  • 0 kudos

BLE_AT_Server application for STM32WB5MM module

Hi,I am looking for the BLE AT server example created using a recent STM32CubeIDE release (1.14.0+) for the STM32WB5MM module. I can't find it.The most similar project I found was to open in STM32CubeIDE 1.14.1 the AT server example provided for the ...

JMarq.1 by Associate III
  • 2089 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.