STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4119 Views
  • 0 replies
  • 3 kudos

Program ST50H with pyOCD

Hi,I'm working with an ST50H based on STM32WLE5 series MCU. Here's the product: https://www.st.com/en/partner-products-and-services/acsip-st50h.html. I would like to be able to flash the device using pyOCD or OpenOCD. However, after installing the ST...

alexemdesgagne_0-1708704076331.png

STM32WB55: Failed read remote feature

Hello,I'm currently developing a Zephyr application and want to use the STM32WB55 chip. For evaluating I use the ST Nucleo WB55RG board. The device is configured as a Bluetooth peripheral using the Zephyr v3.6.0 host stack and the stm32wb5x_BLE_HCILa...

janger by Associate
  • 1583 Views
  • 0 replies
  • 0 kudos

Resolved! stm32wb5mm-dk

HelloI've been recommended the product by the ARROW sales manager, but I'm not getting any documentation or technical help. I'm new to st product and ble.Below are the features I want.1. If you don't do anything for a certain period of time, you will...

About the pairing mode of STM32WB

Excuse me, how can we establish a Bluetooth connection between stm32wb55 as an observer and other broadcasting devices on CubeMX? The current CubeMX can only implement WB as a broadcaster to connect to the app, which is not the pattern required in my...

cxiao.2 by Associate II
  • 2136 Views
  • 1 replies
  • 0 kudos

RTC example folder Freezes at HAL_RTC_Init

I tried the RTC_Alarm example folder, at first it worked out well and I was able to view the output.But when I ran for the 2nd time without any changes in the code the execution stopped at  HAL_RTC_Init ->> (if (HAL_RTC_Init (& RtcHandle)! = HAL_OK))...

Resolved! Can't run SubGHz_Phy_PingPong example on Nucleo WL55JC1

I have a Nucleo WL55JC1 and I'm trying to run the SubGHz_Phy_PingPong example from STM32CubeWL v1.3.0. I am using STM32CubeIde and if I try to build without any modification to the original project the compiler outputs that stm32wlxx_nucleo_radio.h, ...

Catomaior by Associate II
  • 3019 Views
  • 4 replies
  • 0 kudos

Resolved! Pi filter purpose on Lorawan reference design

Hello everyone,In the schematics en.MB1389-WL55JC-highband-E02_Schematic,there's a Pi filter following the RF switch before it links to the SMA connector for the antenna.Upon calculation, I found that the cutoff frequency of this low-pass pi filter i...

OUT.png
Levan by Associate III
  • 1691 Views
  • 1 replies
  • 1 kudos

Resolved! Support for STM32WL3x

Hello, Is there any estimation for when the STM32WL3x will be supported in STM32Cube IDE or STM32CubeMX? Also, is there any estimation for when there will be a dev board available on the market? The SoC STM32WL33C8V6TR looks extremely promising for o...

calin by Associate
  • 1343 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.