2024-02-07 12:50 AM - edited 2024-02-07 4:54 AM
application stopped advertising , with error 0x0C, later to discover it got connected.
is this error indicates I got connected?
does it mean other things too?
thanks
2024-02-07 1:28 AM
@DS.4 wrote:application stopped advertising , with error 0x0C,
So where, exactly, did you see that error code?
From knowing what returned it, you should be able to find what it means ...
2024-02-07 4:48 AM - edited 2024-02-07 4:52 AM
Hi @Andrew Neil
All the document says is that: 0x0C - Command disallowed
Would like to know better what this means and what can it indicate on the system status.
E.g., it is disallowed (cause I am connected) (cause I am disconnected ) ( ... .) ( .... )
if @ST can specify more regarding the reasons, or at least approve my reasoning for this error.
I opened a support ticket as well hopefully to get an answer, but if anyone already has an answer to it or a link to a document with further documentation could help a lot.
2024-02-07 5:35 AM
@DS.4 wrote:All the document says is that: 0x0C - Command disallowed
Which document is that?
2024-02-07 6:44 AM - edited 2024-02-07 6:44 AM
AN5270
Couldn't find the stop advertising/set_non_discoverable command (0xFC81) in BLE core specification
I guess it's a command ST created
2024-02-23 10:22 AM - edited 2024-02-23 10:27 AM
Hello @DS.4
I suggest you look at the Bluetooth core specifications 5.4 Vol 1, Part F.2.12 to find the exact meaning of the 0x0C Command disallowed. Also, searching for the "Command disallowed" will give you a good idea about the use cases related to the 0x0C message.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.