2024-02-24 8:50 PM
2024-02-24 9:58 PM
The above description is incorrect, please correct it here. My usage scenario is: STM32WB55 connects to the APP, and in CubeMX, I use the Custom Template (Enable) in Server profile mode, which defines some GATT applications while BLE Pairing is turned off. Now, due to project requirements, it is necessary to add a BEL peripheral device and connect the STM32WB55 motherboard in pairing mode. The motherboard will obtain some event information from this peripheral device. The observer role mentioned above is unable to establish a connection, which is my mistake and should not be the desired result. Its correct role should be Central, which means that this WB55 motherboard serves both the purpose of connecting to the APP and peripheral devices. I hope to achieve the desired results through the settings of CubeMX. Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.