STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Reconfigure clocks on STM32WB55 BleHeartFreeRTOS

 Hello,Curious regarding clock reconfiguration and MX_XXX_Init on wake up with STM32WB family.I see that in the example BLE_HeartRateRTOS the clock configuration on wake up is blank!Why is that? Doesn't in necessary to do the clock init again? this i...

DS.4 by Senior II
  • 1373 Views
  • 2 replies
  • 0 kudos

Resolved! STM32WL55 middleware SubGHZPHY grayed out

Dear all!I'm working with a custom board. I would like to make a simple application (without Lora). Just sending packets that the device receives from Uart over the air to another device. 1st approch will be only in one direction to keep it simple.So...

robha by Associate
  • 2602 Views
  • 2 replies
  • 0 kudos

BLE Pairing w/ Display only?

Can someone explain to me how the client would know what the server pairing number was if the user used a RNG in the server to create the pairing number?  I certainly see how a fixed number would work as a developer.  But when I try and connect using...

SWenn.1 by Senior III
  • 4145 Views
  • 5 replies
  • 1 kudos

Resolved! using Bluetooth module in project.

Hi  We are using the STM32 in a project and want to use a bluetooth module . I see there are many certified modules out there , but if I use any in a project (even though I dont modify the module at all ),  I have to pay for a bluetooth certification...

Resolved! Debugging STM32WB15CC-CM0+ core

Hi,I am currently attempting to debug the secondary core (cortex-M0+) on the STM32WB15CC board, but I have encountered challenges in doing so. According to the documentation, the boot process is initiated by setting C2BOOT through the primary core (c...

Gaya by Associate
  • 1899 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.