STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! the otbr-agent is not running with stm32wb as RCP

Hi All, I want to create an open thread border router  with raspberry pi 3 and stm32wb55rg :1- first I followed the steps illustrated on this site Connectivity:STM32WB OpenThread Border Router Application - stm32mcu (stmicroelectronics.cn) but i can'...

basmatalbi_2-1709800880316.png basmatalbi_0-1709800338125.png basmatalbi_1-1709800442051.png

Migrate SPBTLE-RF to STMWB1M

We have a product using the SPBTLE-RF module and are looking to migrate the design to use the STMWB1M.  Has anyone done this?  

stst9181 by Associate II
  • 1088 Views
  • 1 replies
  • 0 kudos

how to implement zigbee in stm32f407 board?

Hello, I like to design zigbee -based heath monitoring system, using stm32f407GT6 discovery board, and I plan to add Security in zigbee to protect data against attacks. In my system, I will use three sensors(temperature, Heart Rate (ECG), Blood press...

MH24 by Associate II
  • 4532 Views
  • 1 replies
  • 0 kudos

STM32WB55/35 BLE windows communication

Hello. Any help/guide how to start communication between STM32WB and windows pc via BLE?I want to make wireless temperature probe and i don´t know where to start.

Kowy by Associate
  • 2174 Views
  • 4 replies
  • 0 kudos

Active Endpoint Response missing

Hello,When using device as temperature measurement server and device joins to the network where coordinator is also trust center, joining to the network works fine, but binding not. I wander, why device don't send Active Enpoint Response message when...

eskomj by Associate III
  • 6152 Views
  • 8 replies
  • 0 kudos

Resolved! STM32WL55/STM32WLE5 SubGHz

Hi,I recently started exploring what STM32WL MCUs offer but I don't really understand a few things yet:1. I read somewhere that these STMs are based on SX126x LoRa radio. Is that the case?2. If so, does enabling "SUBGHZ_PHY" in middlewares in CubeIDE...

awocrf by Associate III
  • 7933 Views
  • 1 replies
  • 1 kudos

STM32 WL55JC1 LoRaWAN Class C not working!

Dear community, In the attachments, I am sending You two screenshots, one from the LoRa WAN Network server and the other one from the STM32CubeIDE. We are using two of Your dev boards, one as the LoRa WAN gateway (Nucleo F746ZG) and the other one as ...

fainlaip by Associate II
  • 2787 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.