STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! BlueNRG-M2

Hello,actually, i'm using the bluetooth module BlueNRG-M2 , and i want to know the communication distance in meter please and the length of the antenna .Thank you 

ljm by Associate III
  • 3233 Views
  • 7 replies
  • 0 kudos

STM32WB custom_app.c vs custom_stm.c

Hello....I have generated code with CubeMX for the WB55.  I have read and write on some characteristics with some require authentication.  On one characteristic I have read, write (with authentication) and notification set.  On this same characterist...

SWenn1_0-1708979653285.png
SWenn.1 by Senior III
  • 1341 Views
  • 1 replies
  • 0 kudos

STM32WB5MMG - CPU2 is Blocking Flash operations from CPU1

Hi everybody,Here's a bit of context of my project:I'm using BLE Mesh Template, using Sensor and Generic Models.I'm enabling the USB and the CDC middleware. Thus:I changed the configuration of the SystemClock.The nodes are mostly self-provisioned.One...

rdiaz_ice by Associate II
  • 2138 Views
  • 2 replies
  • 0 kudos

STM32WB1MMC antenna

Hello, is there anything which specifies exactly the copper restriction area (page 11) under the antenna? Thankshttps://www.st.com/resource/en/datasheet/stm32wb1mmc.pdf

marc6h by Associate
  • 877 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WB5x battery-powered BLE device - missing low power APIs?

Dear all,we are trying to build a simple battery-powered BLE device. It should basically measure at intervals and advertise results only (minus the occasional update connection). With limited power resources we would expect to shut down both cores an...

SVogl.1 by Associate II
  • 4034 Views
  • 6 replies
  • 0 kudos

Resolved! BLE 5.4 Audio project guidance

Hello, i have a STM32WBA52CG with a NUCLEO 64 board.I want to utilize the new BLE in speakers. I want a Client phone to broadcast audio to servers -> STM32WBA52CG.First question, does an example sketch exist for this application? Is there some availa...

flamefire by Associate II
  • 5348 Views
  • 7 replies
  • 2 kudos

Resolved! wb55 can't wakeup from stop2 by LPTIM

hello everyone!from the link Solved: STM32U5 Can't exit STOP2 mode with LPTIM - STMicroelectronics Communityit is possible to make LPTIM work in stop2and there is a macro,__HAL_RCC_LPTIMx_CLKAM_ENABLE(), where x can be 1, 3, or 4. but in my project,(...

Cchn.1 by Associate II
  • 1392 Views
  • 1 replies
  • 0 kudos

STM32WB Reset issue

Hi,   I am Firmware Engineer and I'm using stm32WBMMG controller in custom board. Here, I can program it and is running the application right but it resets again and again and we found it by programming the RCC-> CSR control and status of reset flag ...

BT.2 by Associate II
  • 1436 Views
  • 1 replies
  • 0 kudos

STM32WB5 USB CDC not working after STOP mode

Hello,I am trying to use the USB virtual com port on an STM32WB5MMG. After trying to go into any of the stop modes, I cannot get the virtual com port to work again. (I am using the RTC alarm to wake up the MCU from stop mode and it wakes up fine)I ha...

Dracu by Associate II
  • 2397 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.