2024-03-26 2:09 AM - edited 2024-04-02 11:28 PM
Hello everyone,
I am working with STM32WB55RG board to make a custom profile that sends a read request from mobile app to the board to communicate with STM32F7 via SPI. F7 contains the data that has to be sent to the mobile app.
I have been trying to figure how to integrate BLE and SPI in my code. I have used the snippet codes of SPI and it works fine.
It seems to be very difficult and the resources and tutorial aren't that straight forward like I wanted them to be. I am just not able to build the connection between the app and SPI.
@TDK @KDJEM.1 @Issamos @Remy ISSALYS @Remi QUINTIN Can you please explain me how to connect the mobile interrupt to enable the SPI.
Thanks in advance!
Solved! Go to Solution.
2024-04-17 2:04 AM
Hello @Pallavi
I suggest you refer to the BLE_p2pServer to understand how the application commend is communicating with the Led of the Board. After that, you can modify the example by adding a task that start the SPI part and this task depend on the message coming from the Mobile app.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-17 2:04 AM
Hello @Pallavi
I suggest you refer to the BLE_p2pServer to understand how the application commend is communicating with the Led of the Board. After that, you can modify the example by adding a task that start the SPI part and this task depend on the message coming from the Mobile app.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-17 4:34 AM
Thank you so much!
Will try to implement this and revert back to you if I have any doubt.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.