2024-04-04 8:49 AM
Hi,
My application (WB15CC) stays most of the time in standby mode transmitting the advertainment packet. After a couple of minutes, the advertainment packet must be updated. When I try to update the packet after waking up from the standby mode, the firmware hangs on any of the GAP API routines, e.g. aci_gap_set_non_discoverable(), aci_gap_set_discoverable() or aci_gap_update_adv_data().
I've edited the startup code by adding the CPUcontextSave and CPUcontextRestore routines, similar to the BLE_HeartRate example, to restore the CPU context when waking up from the standby mode. Indeed, the CPU is restored correctly I am able to register a new task inside the UTIL_SEQ_PostIdle() routine, however my task can't update the packet.
Can someone elucidate me what are the steps to update the advertisement packet when coming out of the standby mode?
2024-05-15 9:44 AM
Hello @rs-dp
To update the advertising data without stopping the advertising, I suggest you use the command ACI_GAP_UPDATE_ADV_DATA.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.