NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello, I have a problem running any project in STM32CubeIDE v1.7.0When I press 'Run' I usually get "Launching: Performing pre-launch check..." and it just hangs there.Sometimes it gets past that, and then I get the following errorError in final launc...
Hi there, We want to stream video at a reasonable quality (HD) using the STM32WL, we were thinking on implementing this feature using LoRa, but looks like Sub-GHZ system isn't no capable for transmitting video. What other methods can we use that can ...
Hello Is it possible to use the P2P server example in stm32wb55 examples to add my own service and Characteristics and then be able to access my data on the STM32 sensor app. For example I want to add a sensor then send that data to my phone using th...
For a project im working on i need to be able to record sound with a battery powered microcontroller and send it to an RPi. I saw that the STM32WB was capable of this but can anyone tell me if i will be able to receive and process the audio file on ...
Hi, I have two NUCLEO-WL55JC1 boards with me. I want to make one board as a end device and one board as a gateway. I found end node example with in firmware package of STM32WL but not found any example for gateway.Is there any gateway example availab...
Hi All, I can import STM32WB5MM-DK Zigbee_OnOff_Server_Coord application into STM32CubeIDE and can compile and debug, however, I would like to see .ioc file to understand more clearly how to set the clock and pins etc. I wonder if there is any place ...
Hello, We're wondering about the Next_State_Systime field in the end_of_radio_activity events - what kind of time unit is used for it, and how to make a use of it on application side.Long story short, we'd like to avoid some noise sensible operations...
Hello,I have a NUCLEO-WL55JC1 development board that I am trying to have communicate over subGHz RF.After configuring the RF module, I am trying to read what interrupts are generated based on different stimuli. To accomplish this, I set a breakpoint ...
Hello ....I have an apk that seems to lose comms with a server. We have not been able to make it periodic or obvious as to the reason. We would like the server to timeout after 30 seconds of not receiving read/write rqsts from the client and force ...
For a project for one of our customers, we use STM32WB15CCU6 microcontrollers on a custom board. The boards are returning from the field with several of the option bytes of the microcontroller set to a different value than they were programmed with. ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.