NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello ST experts,I hope this message finds you well!I am writing to request your support for a project involving the Nucleo-WL55JC. I have successfully communicated between two Nucleo boards using RF communication with the SUBGHZ protocol (not LoRa)....
Hi ST support team,I'm trying to implement OTA in my application using the BLE-OTA bootloader firmware and test it using BLE sensor application running on a mobile device. I have successfully tested the BLE-OTA using the heart rate sensor OTA applica...
I'm using STM32Cube_FW_WL_V1.3.0and trying to generate LoRaWAN End Node FreeRTOS. I precedently set in file se-identity.h values for LORAWAN_APP_KEY,LORAWAN, LORAWAN_NWK_KEY,LORAWAN_JOIN_EUI, as shown in the guide and everything went fine.Now I want ...
Hi,the STM32WL55's reference manual states:> BW[DSB] > BR + 2 x frequency deviation + frequency errorHowever, in the SubGHz_Phy_Per example, FSK is configured as follows: #define FSK_FDEV 25000 /* Hz */ #defin...
For your informationSizeof is used in place of strlen and my coordinator receive a \0x00 at the end of the string !!when i generate code with MX generation tools, in function : in red old code in green new code void APP_ZIGBEE_ConfigBasicServer(void)...
Hello developers,I am currently developing all-in-one AT slave firmware for STM32WLE5CCUX, which can handle both LoRaWAN and Sigfox AT commands. I have successfully implemented and tested AT slave drivers for LoRaWAN and Sigfox using the video linked...
Could you add NVM option for zigbee stm32WBA in cubeMX ?It's essential for developement of application (persistence and coord association...)thanks
Hi,In a centralized network, the coordinator is the only entity able to permit network joining. If the coordinator power cycles, and starts up from persistence, does it maintain its coordinator status?In my testing setup, when I power cycle the coord...
Hello everyone,I am working with a STM32WB5MMDK. I want to use the USART to print a message on Tera Term but i just have inversed triangles instead of "Hello world". I checked and both Tera Term and USART1 have the same parameters (baud rate, etc). I...
Hello, I have some trouble with a STM32 MCU. I was playing with the radio firmware and delete it. From now on, I'm unable to reprogram it, I always get this kind of error ( FUS_STATE_ERR_UNKNOWM) : FUS seems to be in bad state : By comparaison wi...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.