NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Can anyone tell me how to do it without wasting days to simply compile a project from the repo:https://github.com/STMicroelectronics/STM32CubeWBalthough if I import any ìxample from stm32cubeide when I compile it tells me that there are missing libra...
Hello. I am developing a BLE HID device using the STM32CubeWB MCU Firmware Package, but when I try pairing => disconnect => pairing, pairing fails. I have an implementation like this, is there a problem?We have the following data in adv_data, whic...
Hello, where I can find info about STM32WB55CG (USB dongle) usage description and what Blue Tooth USB dongle can be used with STM32WB5MMG module ?
Hi I am testing with STM32WL55CCU6.When I use only uart1, uart1 works well.but when I use uart1 and RF(LoRa) send, MCU does not work.I coded that MCU transmit some message using uart to terminal per second.MCU continues to work fine.but I added some...
hi ALL I bought three stm32 Lora HF band sensor and gateway pack. I would like to communicate by connecting one gateway (nucleo-F746) and three end nodes (nucleo-L073) directly (no server, no site). Is it possible? And please tell me the example co...
Hello,I work on a simple config with stm32CubeMX with 2 endpoints on stm32wba54kgu6,Endpoint 1 with cluster on/off receiving command clientEndpoint 2 running as cluster temperature server.I use ZigbeetoMqtt coordinator.When i use router mode, i can ...
Good morning,I am trying to follow the RTC_LSI calibration example project for the P-NUCLEO-WB55.https://github.com/STMicroelectronics/STM32CubeWB/blob/master/Projects/P-NUCLEO-WB55.Nucleo/Examples/RTC/RTC_LSI/Src/main.cThe GetLSIFrequency function h...
Hello, I have a question about the internal antenna of the STM32WB55CGU6.First of all, does it have the internal antenna? And if so, what is the range of it? Thanks
Hey,I working on a project with the following goal: setup one central coordinator and let multiple sleepy end devices send sensor data periodically. For development I am trying to alter the code of the Zigbee_TempMeas_Client_Router/Zigbee_TempMeas_Se...
Hi there,if i try to set my stm32wb55cg into standby, it seems to only work if the RFWakeupCLK is HSE-DIV1024void PeriphCommonClock_Config(void) { RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0}; PeriphClkInitStruct.PeriphClockSelection = RCC_...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.