STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

1.8V VDDA-Vref Voltage

Hello, I have a custom STM32WB55 board and for custom purposes, I want to use VDDA=1.8 V and Vref=1.8 V from same Reference IC. According to datasheet, I can decrease VDDA from 3.3 V to as low as 1.62 V but I just wanted to make sure that it won't ca...

Makif by Associate
  • 1299 Views
  • 1 replies
  • 0 kudos

Modify a project base ble_pheripal_lite

When I create my basic project   choose from ST32CUNE ide the example  ble_pheripal_lite all is ok .The problems arrive when I want add  for example a new periperal how ADC .... How can add in the driver the adc the stm32wbxx_hal_adc.c!!!!Thanks

battellino_0-1719209291918.png

Resolved! CubeMx HeartRate Needs Not Avail Cube_FW_V1.20.0

HelloI have CubeMx v6.11.1.Am trying to start a BLE_HeartRate project targeting P-Nucleo-WB55-Nucleo, and CubeMx is needing STM32Cube_FW_WB_V1.20.0This is not available at the ST website. Can you send me this or tell me how to create this project usi...

GRama.2 by Associate III
  • 4538 Views
  • 6 replies
  • 0 kudos

Resolved! STM32WL33KB 2.4GHz frequency band support

The datasheet of STM32WL33KB states that the frequency bands 159-185 MHz, 413-479 MHz, 826-958 MHz are supported.However, the website mentions that "For greater flexibility, it supports wide frequency bands from 100 MHz – 2.4 GHz". Can I get some cla...

image.png leahjoseph_1-1718883117832.png

Resolved! Hardware/fuse disabling OTA updates for security?

Hi All!We have a requirement to disable OTA updates either via hardware or by settings a fuse, this is due to the need for a low-maintaince, low-complexity, high-security method to prevent updates to those without physical access to the device.Is the...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.