NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi Team,Am designing a BLE module using STM32WB55CEU6 for an IoT audio streaming project. Can somebody please help me in verifying the RF portion of schematics and layout. We are using an IPEX connector on board for BLE antenna and the signal is conn...
Hello, I need your kindly support for this application.I would like to do a code for the STM32WB5MM-DK where the Bluetooth have a service with the following characteristics:ServiceCharacteristic 1: Read and Notify a random number from 0 to 100 (later...
While attempting to identify an issue with reading and writing to emulated EEPROM, I have identified a bug in V7.0.0 of the X-CUBE-EEPROM source code.This was identified in the STM32WB version of `flash_interface.c` with `DUALCORE_FLASH_SHARING` defi...
Hi,In my product, I use the STM32WB5MMG module as Bluetooth link with the rest of the product.The STM32WB5MMG module is configure as Client.But during the discovery procedure, I always go to :- SVCCTL_App_Notification -> case HCI_VENDOR_SPECIFIC_DEB...
The following are the steps i am following to access ram2 (my Microcontroller documents - https://www.st.com/en/microcontrollers-microprocessors/stm32wle5cc.html) See the linker script ,how they have defined ram2 in my linker script they have def...
Hello. If I write the protocol stack to an address different from the original address, will the protocol stack work properly? The firmware I wrote is stm32wb5x_Ble_Mac_802_15_4_fw.bin, and I wrote it to 0x080B1000 when it should have been written to...
When I was debugging, I found that the program got stuck in SHCI_C2_BLE_Init, and it neither returned success nor failure.What is the reason for this? I correctly burned FUS and protocol stack when I confirmed, and the version also corresponds.
Any idea to open the MX and see how clock is setup?This project was created on TrueSTUDIO as reported in the error message (old_MX_IDE.jpg). Hit CONTINUE or MIGRATE give same error message (continue.jpg).Seem it says needing MX 5.3.0 and FW_F1 V1.8....
Hey,im developing a zigbee sleepy end device. The device is supposed to periodically send sensor values (max length of 512bytes) read via I2C to the coordinator using the custom cluster. I use the HW_TS to trigger the sensor readings and sending the ...
Where can I find the st-nucleo-lora-gw-atfw-v2.0.2.bin for the NUCLEO-F746ZG board
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.