2021-11-07 11:06 PM
Hi I am testing with STM32WL55CCU6.
When I use only uart1, uart1 works well.
but when I use uart1 and RF(LoRa) send, MCU does not work.
I coded that MCU transmit some message using uart to terminal per second.
MCU continues to work fine.
but I added some code that MCU transmit some data using LoRa to remote device per second.
A message is output to the terminal a few times, then no more output,
and the mcu does not work.
I think there are some problem between uart and RF.
Does your library 1.1.0 have some problem?
Below are some part of my code.
1. init
MX_GPIO_Init();
MX_I2C2_Init();
MX_SUBGHZ_Init();
MX_USART1_UART_Init();
MX_USART2_UART_Init();
MX_I2C3_Init();
MX_RTC_Init();
MX_TIM16_Init();
/* USER CODE BEGIN 2 */
HAL_TIM_Base_Start_IT(&htim16);
MX_SubGHz_Phy_Init();
2. uart callback
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart) {
if (huart->Instance == USART1) {
loadReceiveConsoleData(uart1_data);
HAL_UART_Receive_IT(&huart1, &uart1_data, 1);
}
else if(huart->Instance == USART2) {
HAL_UART_Receive_IT(&huart2, &uart2_data, 1);
}
}
3. rf init
void SubghzApp_Init(void)
{
/* USER CODE BEGIN SubghzApp_Init_1 */
/* USER CODE END SubghzApp_Init_1 */
/* Radio initialization */
RadioEvents.TxDone = OnTxDone;
RadioEvents.RxDone = OnRxDone;
RadioEvents.TxTimeout = OnTxTimeout;
RadioEvents.RxTimeout = OnRxTimeout;
RadioEvents.RxError = OnRxError;
Radio.Init(&RadioEvents);
// USER CODE BEGIN SubghzApp_Init_2
Radio.SetChannel(RF_FREQUENCY);
Radio.SetTxConfig(MODEM_LORA, TX_OUTPUT_POWER, 0, LORA_BANDWIDTH,
LORA_SPREADING_FACTOR, LORA_CODINGRATE,
LORA_PREAMBLE_LENGTH, LORA_FIX_LENGTH_PAYLOAD_ON,
true, 0, 0, LORA_IQ_INVERSION_ON, TX_TIMEOUT_VALUE);
Radio.SetRxConfig(MODEM_LORA, LORA_BANDWIDTH, LORA_SPREADING_FACTOR,
LORA_CODINGRATE, 0, LORA_PREAMBLE_LENGTH,
LORA_SYMBOL_TIMEOUT, LORA_FIX_LENGTH_PAYLOAD_ON,
0, true, 0, 0, LORA_IQ_INVERSION_ON, true);
Radio.SetMaxPayloadLength(MODEM_LORA, MAX_APP_BUFFER_SIZE);
int random_delay = (Radio.Random()) >> 22; // 10bits random e.g. from 0 to 1023 ms
// starts reception
Radio.Rx(RX_TIMEOUT_VALUE + random_delay);
UTIL_SEQ_RegTask((1 << CFG_SEQ_Task_SubGHz_Phy_App_Process), UTIL_SEQ_RFU, RF_Process);
/* USER CODE END SubghzApp_Init_2 */
}
Can you resolve the problem??
I added all source
Please help me~~~~~
2021-11-08 12:53 AM
Hi @Son, Dong-Seong
On my point of view the timer are not working in the projet you have shared ? The timer_if.c is not implement like under LoRaWAN\LoRaWAN_End_Node\Core\Src\timer_if.c. Do you know why ? Did you create you projet with CubeMX ?
Bruno
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-11-09 8:37 PM
Hi. Bruno_ST
Thank you for your response.
I didnot use timer_if.c for timer.
I use timer16 for only HAL_Delay().
Should I use the timer_if.c file for the timer of RF
I created my project with CubeMX on STM32CubeIDE.
If there is somthing wrong in my code, please let me know exactly how to fix it.
Please help me.
thank you.
2021-11-09 11:06 PM
in stm32wlxx_hal_subghz.c file, there is the function as blow
HAL_StatusTypeDef HAL_SUBGHZ_ExecSetCmd(SUBGHZ_HandleTypeDef *hsubghz,
SUBGHZ_RadioSetCmd_t Command,
uint8_t *pBuffer,
uint16_t Size)
In the fucntion, I commeted out LL_PWR_UnselectSUBGHZSPI_NSS();
then the program was not halt, and worked well
what is the funtion - LL_PWR_UnselectSUBGHZSPI_NSS(); ?
Is it necessary?
I want to know why that function makes program halted.
please let me know if I can comment out that function,
or if absolutely necessary, how to make it work without stopping the program.
Please help me
2021-11-09 11:49 PM
Hi @Son, Dong-Seong
Yes, i think timer_if.c is needed for the RF. Otherwise i guess that you won't wakeup.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-05-22 6:07 AM
Hello,
I do have a quite similar issue...
I started my project from the end-node example (single core) and adapted it to my context; meaning that I removed the sequencer and util_timer (because I already had my own) and just make periodic calls to LmHandlerProcess as in the provided example.
Everything works find except that, from time to time, I do lose the UART communication when Lora transmissions occur.
UART is used in interrupt mode, initiated by a call to HAL_UART_Receive_IT (re-issued each time a character is received), and when LoRa processing occur the UART status is no more in the receive mode (bit b1 of HAL_UART_StateTypeDef no more set).
If I disable LoRa, UART works forever!
The workaround I've found so far is to check UART status periodically, and re-issue a HAL_UART_Receive_IT if not in the busy state. But this is not very clean, and I would like to undestand what occurs in the LoRa Firmware able to cause that.
I've not been able to identify yet anything that could explain this behavior in the LoRa stack (but it is quite heavy).
Any idea or suggestion?
Thanks
JYL
2024-06-10 5:09 AM
I'm facing the same problem. I'm using FreeRTOS with LoRa and UART1 of STM32WL5JCI. The UART reception works fine, until I send a LoRa message it stops receiving characters.
@JLojo @Son, Dong-Seong Did you manage to solve it? If you can help me, I'd appreciate it!
2024-06-10 5:41 AM
Hi Rick88,
Actually I did not really solve the issue but found a workaround:
I simply check periodically if the UART is still in the ready mode by calling HAL_UART_GetState and checking if bit b1 is set, if not set I call again HAL_UART_Receive_IT.
Not very clean, but actually it works and allow me to continue receive data on the UART!
regards
JYL
2024-06-19 11:55 AM
Hi @JLojo,
I did it the same way you said! So far everything works. But I'm thinking about using UART2, I'm afraid that UART1 will stop working.
Thank you very much!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.