2024-06-20 4:33 AM
The datasheet of STM32WL33KB states that the frequency bands 159-185 MHz, 413-479 MHz, 826-958 MHz are supported.
However, the website mentions that "For greater flexibility, it supports wide frequency bands from 100 MHz – 2.4 GHz".
Can I get some clarification as to whether 2.4 GHz is supported or not?
Solved! Go to Solution.
2024-06-20 9:20 AM
Hello @leahjoseph and welcome to the ST Community :smiling_face_with_smiling_eyes:
The 2.4GHz is supported only for on the Wake-up radio receiver and not for the Ultra-low power Sub-1GHz RX/TX transceiver. The STM32WL33 include two separated Radio modules:
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-06-20 9:20 AM
Hello @leahjoseph and welcome to the ST Community :smiling_face_with_smiling_eyes:
The 2.4GHz is supported only for on the Wake-up radio receiver and not for the Ultra-low power Sub-1GHz RX/TX transceiver. The STM32WL33 include two separated Radio modules:
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.