STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! [Zigbee] Router node implementation

Zigbee PRO specification mentionsI found this function in AN5500: When I try to implement this function, I get a compiler error for 'undefined reference'. I checked zigbee_core_wb.c and indeed there is no implementation for this function. The questio...

0693W00000LwhlKQAR.png 0693W00000LwhlPQAR.png 0693W00000LwhmhQAB.png
DA.5 by Associate
  • 2905 Views
  • 4 replies
  • 0 kudos

Resolved! Audio on STM32WB55CG?

Hello @STTwo-32 ! Thank you so much for clarifying everything! I am really thrilled with the STM32WBA Nucleo board. Could you please let me know, if it is compatible with the FP-AUD-BVLINKWB1 pack? If not, are there any code examples on how to implem...

Skfir by Senior
  • 2749 Views
  • 4 replies
  • 3 kudos

Resolved! 2.4GHz frequency band support

Hello,I am looking for a low power STM32 MCU that can transmit 2.4GHz RF signals. Since STM32WBA and STM32WB support bluetooth, can it be used to transmit raw 2.4GHz signals as well as bluetooth.It is used to communicate with a cnc controller. 

Resolved! Audio on STM32WB55CG?

Hello everybody!There is a question on bluetooth which I would love to explore. The point is, some time ago I developed a navigation device for visually impaired people, that had a pair of mikes, a pair of headphones and a DSP. Everything was more or...

Resolved! BLE with audio and signal processing

Hi,I am looking for a MCU with BLE5 and audio. If BLE5 is not available with audio, then I will get compromised with Classic bluetooth. If such an MCU has signal processing capability then it will be an added advantage for me, so that I will not use ...

Resolved! P-NUCLEO-LRWAN2 - gateway firmware sources

 Hello,The firmware for the P-NUCLEO-LRWAN2 gateway is currently provided as a binary file named "st-nucleo-lora-gw-at-fw-v2.1.7-eu868-TTN.bin." I am very interested in obtaining access to the source code to develop a modified version of the firmware...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.