2024-07-05 2:59 AM
Hello,
I am looking for a low power STM32 MCU that can transmit 2.4GHz RF signals. Since STM32WBA and STM32WB support bluetooth, can it be used to transmit raw 2.4GHz signals as well as bluetooth.
It is used to communicate with a cnc controller.
Solved! Go to Solution.
2024-07-05 3:43 AM
Hello @leahjoseph
The STM32WB/WBA support multiple protocols that are Bluetooth® Low Energy 5.4, IEEE 802.15.4 communication protocols, Zigbee, Thread and Matter.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-05 3:43 AM
Hello @leahjoseph
The STM32WB/WBA support multiple protocols that are Bluetooth® Low Energy 5.4, IEEE 802.15.4 communication protocols, Zigbee, Thread and Matter.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.